Skip to main content
RPari.1
Associate
Oct 7, 2020 12:35 AM UTC
Question

SPC58EC DISP not build aplications

I'm loading aplication's SPC58EC DISP, and debugging, but if I change the main.c this is the 9 problens. What it's, please?

Another problem is that if I change and build the project, the changes not appear

in the UDESTARTERKIT.

    This topic has been closed for replies.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    Oct 7, 2020 2:08 PM UTC

    Hello ,

    All the applications based SPC58EC DISP are built, flashed and tested on our continuous integration.

    Could you detailed your problem ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    RPari.1
    RPari.1Author
    Associate
    Oct 7, 2020 3:58 PM UTC

    I only had created one variable in main.c

    If i change anyfing in main.c have 9 problens.

    We see that the project folder is only read.

    If I uncheck box read only in the folder , after building it's return to read only.

    Erwan YVIN
    ST Technical Moderator
    Oct 13, 2020 9:32 AM UTC

    Hello ,

    The problem can come from CDT. (C/C++ Development Tooling) Symbol Issues on the compiler.

    could you send me the screenshot ?

    could you detail your issue and show the errors logs ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    RPari.1
    RPari.1Author
    Associate
    Oct 13, 2020 10:58 AM UTC

    0693W000004JfwtQAC.png0693W000004JfwjQAC.pngHello,

    below it's 9 problens,

     If I change the main.c and build the sisten not such the directory,

    I see again if only write in the main one variable for example:

    the SPC5studio don't creat the code.

    Erwan YVIN
    ST Technical Moderator
    Oct 16, 2020 9:39 AM UTC

    Hello ,

    Ok , i see your error logs ;)

    Have you clicked on generate before compilation ?

    could you export and send me your application if there is no confidential code?

    What is your installation details ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.