Skip to main content
SKara.7
Associate III
Jun 23, 2022 5:26 PM UTC
Question

SPC584xx CAN Transmit Message sending wrong data for one sample - Intermittent Issue

Hello ,

I am facing an issue wherein the CAN transmit message is sending wrong data for one sample in between the transmission. Please see the below screenshot.

0693W00000NsdjFQAR.pngT3_C1_ECU_SCIMO_PE_CTRL_MOT is a transmit frame with a cycle time of 10ms.

The transmission baudrate is 1Mbps.

As highlighted in the screenshot, the transmit message is sending garbage wrong values for 1 cycle and returns to the original value assigned from the applicaiton software.

Microcontroller platform = SPC584xx

Development toolcahin = SPC5Studio 6.0.0

Low Level Drivers = Generated by SPC5Studio

RTOS used = FreeRTOS

Please can anyone help me to understand where the issue is?

Best regards,

Sreejith

This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Jun 30, 2022 8:17 AM UTC

Hello ,

I think that a deep debug is needed.

Have you checked or enabled ECR register (Transmit Error Counter or CEL)?

Do use Threads in FreeRTOS ?

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SKara.7
SKara.7Author
Associate III
Jun 30, 2022 8:39 PM UTC

Hi Erwan,

Thanks for the response.

I am not sure about ECR register.

I am using multiple Tasks of different time periods (10ms, 50ms, 100ms, 200ms and 1000ms) using FreeRTOS.

Please find attached the configuration.xml file that I am using with the application.

Best regards,

Sreejith