Skip to main content
R. M.
Associate II
May 7, 2021 9:45 AM UTC
Solved

Spc584b-Disp in RESET and cannot connect to it

Hi All ,

I flashed the board Spc584b-Disp with a SW that had a watchdog reset happening .

When I repower the Board and try to connect to it to reflash ,the RESET LED4 is alawys ON ,and the UDE gives an error PpcJtagTargIntf: No JTAG client found !

Message from component 'PpcJtagTargIntf' :

Can't connect target !

Message from component 'PpcJtagTargIntf' :

No JTAG client found !

Please check:

- target power supply

- JTAG cable connection

- target configuration

I know it is not the UDE STK 5.2 Problem because I reinstalled the drivers and the UDE STK and I can connect to other Spc58 Boards using it .

The problem is with the Board ,I can see the SW running at power ON (LEDS Indication) and then going through WDG RESET forever .

Is there a way I can fix this ?

All Board Jumpers are in Default setting.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    May 11, 2021 8:39 AM UTC

    Hello R.M. ,

    maybe you are in Reset Escalation , Could you hold reset button and try to connect in order to take the hand on PLS ?

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    May 11, 2021 8:39 AM UTC

    Hello R.M. ,

    maybe you are in Reset Escalation , Could you hold reset button and try to connect in order to take the hand on PLS ?

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    R. M.
    R. M.Author
    Associate II
    May 11, 2021 10:22 AM UTC

    Thank you ,That actually Worked !