Skip to main content
Associate
Aug 4, 2023 12:57 PM UTC
Solved

SPC58

We are using SPC58NH-disp.
We are developing a software that we want to print the data we receive over CAN-FD to the screen with TCP.
We are using a Simple TCP Echo Server Demo for TCP.
Data flow takes place indefinitely and in indefinite numbers.But suddenly the device is locked.
Either, Can-fd data is transmitted endlessly when the Ethernet socket is not plugged in.
However, when the socket is inserted, the device is locked even if the connection is not established.
Can you help with this crash?

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Aug 23, 2023 9:50 AM UTC

Hello,

Did you solve your issue?

i recommend to use a debugger and check PC,R13,R14 with Stack history

                  Best Regards

                                  Erwan

               Best Regards

                               Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Aug 23, 2023 9:50 AM UTC

Hello,

Did you solve your issue?

i recommend to use a debugger and check PC,R13,R14 with Stack history

                  Best Regards

                                  Erwan

               Best Regards

                               Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SPC58NHAuthor
Associate
Feb 12, 2024 8:13 AM UTC

Hello Erwan,

Thank you for your answer.

According to your answer, when I turned on the device, the device locked at the point in the image.

Can you help me with the solution?

Best Regards

SPC58NH_0-1707725559240.pngSPC58NH_1-1707725570371.png

 

Erwan YVIN
ST Technical Moderator
Feb 12, 2024 1:22 PM UTC

Hello ,

it is a data abort ..check R13, R14 with your debugger 

it will point where the data abort happenned.

            Best Regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.