Skip to main content
Guglielmo Spina
Associate
Feb 5, 2018 1:39 PM UTC
Question

SPC570S40 start in RUN0 mode with debugger

Posted on February 05, 2018 at 14:39

Hi ,

I'm new and I 'm developing on SPC570S40E1.

I've a demo board and my final target board.

When I try to debug my application I've 2 different behavior between  demo board and final target:

 on demo board during clock initialization I see by ME_GS register that the system is DRUN mode, while , on my final target, sw go in irqSysHalt called  by spc_clock_init SPC5_CLOCK_FAILURE_HOOK because system mode is RUN0.

My demo board is SPC570S-DISP , my target is the same  micro 64 pin and I use UDESTK with microUSB.

On the final target , after load the program, if I power on the board, the program run correctly, while with Debugger don't  run because is locked in irqSysHalt.

#spc570s40e1 #ude #udestk
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Feb 6, 2018 10:35 AM UTC
    Posted on February 06, 2018 at 11:35

    Hello Guglielmo ,

    No problem is noticed on

    SPC570S-DISP.

    Could you check the application SPC570Sxx_RLA SERIAL Test Application for Discovery located in SPC5Studio ?

    Did you use the same way of debugging (PLS) for your final board ?

      Best regards

                    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Guglielmo Spina
    Associate
    Feb 7, 2018 10:59 AM UTC
    Posted on February 07, 2018 at 10:59

    Hello Erwan,

    Yes, on final board I'm using SPC5-UDESTK PLS USB/JTAG adapter