Skip to main content
BEdel.1
Associate
Feb 18, 2020 1:33 PM UTC
Question

SPC570s-DISP board: FlexCAN sends bad frames independent of CAN parameters

Hello,

I have similar problem with the SP570S-DISP board as described here:

https://community.st.com/s/question/0D50X0000ArRejNSQS/spc570-can-outputs-bad-frame-independent-of-frame-parameters

My Configuration: 250KBaud, 16Tq, Sample-point=75%, XOSC 40MHz, CAN_clk 40 MHz, V_ext=12V/VDD_HV_IO=5V, Vector VN1610+CANoe running, 120 Ohm on both sides, ID=0x135, Data={0xAA, 0x55, 0x00, 0x00, 0xAA, 0x55, 0x00, 0x00} DLC=8.

 Clock settings:

/* Setting the system dividers to their final values.*/
 /*
 * b0 : DE = 0b1 enable divider
 * b9-15 : DIV (Divider is DIV + 1)
 */
 /* System clock 0 divider */
 MC_CGM.SC_DC0.R = 0x80000000UL;
 /* System clock 1 divider */
 MC_CGM.SC_DC1.R = 0x80010000UL;
 /* System clock 2 disabled */
 MC_CGM.SC_DC2.R = 0UL;
 
 /* Pit clock divider 5 */
 MC_CGM.AC0_DC0.R = 0x80040000UL;
 /* SAR ADC clock divider 25 */
 MC_CGM.AC0_DC1.R = 0x80180000UL;
 /* CTU clock divider 25 */
 MC_CGM.AC0_DC2.R = 0x80180000UL;
 /* DSPI clock divider 4 */
 MC_CGM.AC0_DC3.R = 0x80030000UL;
 /* LinFlex clock disabled */
 MC_CGM.AC0_DC4.R = 0UL;
 /* eTimer clock divider 4*/
 MC_CGM.AC0_DC5.R = 0x80030000UL;
 /* FlexCAN clock divider 1 */
 MC_CGM.AC1_DC0.R = 0x80000000UL;
 
 /* Setting the clock selectors for PIT, SAR, CTU, DSPI, LinFlex, eTimer: PLL_0 */
 /*
 * b4-7: SELCTL (Auxiliary clock source selection control)
 * */
 MC_CGM.AC0_SC.R = 0x02000000UL;
 /* Setting the clock selectors for FlexCAN: XOSC (external oscillator) */
 MC_CGM.AC1_SC.R = 0x01000000UL;
 /* Setting the clock selectors for PLL_0: XOSC (external oscillator) */
 MC_CGM.AC2_SC.R = 0x01000000UL;
 /* Setting the clock selectors for PLL_1: XOSC (external oscillator) */
 MC_CGM.AC3_SC.R = 0x01000000UL;

FlexCAN settings:

uint8_t mb_index = 0;
 
 /* set peripheral clock mode.*/
 cpu_set_peripheral_clock_mode(79U, 0x12);
 
 /* external clock source */
 FLEXCAN_0.CTRL.B.CLK_SRC = 1U;
 
 /* Empty all mailboxes */
 for (mb_index = 0; mb_index < 8U; mb_index++) {
 FLEXCAN_0.MB[mb_index].MB_CS.R = 0UL;
 FLEXCAN_0.MB[mb_index].MB_ID.R = 0UL;
 FLEXCAN_0.MB[mb_index].MB_DATAL.R = 0UL;
 FLEXCAN_0.MB[mb_index].MB_DATAH.R = 0UL;
 }
 
 /* Enable the device.*/
 FLEXCAN_0.MCR.B.MDIS = 0U;
 
 while (0 == FLEXCAN_0.MCR.B.LPM_ACK)
 ;/* wait until module is enabled */
 
 FLEXCAN_0.MCR.B.FRZ = 0b1;
 FLEXCAN_0.MCR.B.HALT = 0b1;
 
 while (0 == FLEXCAN_0.MCR.B.FRZ_ACK)
 ;/* enter freeze mode */
 
 FLEXCAN_0.MCR.B.MAXMB = 7U;
 
 FLEXCAN_0.MCR.B.SUPV = 0b0; /* deactivate super-visor mode */
 FLEXCAN_0.MCR.B.SRX_DIS = 0b1; /* No self reception*/
 FLEXCAN_0.MCR.B.FEN = 0b0; /* No Fifo */
 FLEXCAN_0.MCR.B.AEN = 0b0; /* No Abort enable */
 FLEXCAN_0.MCR.B.WRN_EN = 0b1;
 FLEXCAN_0.MCR.B.LPRIO_EN = 0b0; /* no prio */
 
 (void) FLEXCAN_0.TIMER.R; /* Unlock message buffer */
 
 /* RX MB initialization.*/
 for (mb_index = 0U; mb_index < 4U; mb_index++) {
 FLEXCAN_0.MB[mb_index].MB_CS.B.CODE = 4U;
 }
 
 /* TX MB initialization.*/
 for (mb_index = 4U; mb_index < 8U; mb_index++) {
 FLEXCAN_0.MB[mb_index].MB_CS.B.CODE = 8U;
 }
 
 FLEXCAN_0.CTRL.B.PSEG1 = 5U;
 FLEXCAN_0.CTRL.B.PSEG2 = 3U;
 FLEXCAN_0.CTRL.B.PROPSEG = 4U;
 FLEXCAN_0.CTRL.B.PRESDIV = 9U;
 FLEXCAN_0.CTRL.B.RJW = 1U;
 FLEXCAN_0.CTRL.B.SMP = 0b0;
 
 FLEXCAN_0.CTRL.B.LBUF = 0b1; /* Lowest buffer first */
 FLEXCAN_0.CTRL.B.TWRN_MSK = 0b1;
 FLEXCAN_0.CTRL.B.RWRN_MSK = 0b1;
 FLEXCAN_0.CTRL.B.BOFF_MSK = 0b1;
 FLEXCAN_0.CTRL.B.ERR_MSK = 0b1;
 FLEXCAN_0.CTRL.B.LOM = 0b0; /* listen-only */
 FLEXCAN_0.CTRL.B.LPB = 0b0; /* loop back */
 FLEXCAN_0.CTRL.B.TSYN = 0b0;
 
 FLEXCAN_0.MCR.B.FRZ = 0U;
 
 while (1 == FLEXCAN_0.MCR.B.FRZ_ACK)
 ;/* leave freeze mode */
 
 /* IRQ setting for TX buffers */
 FLEXCAN_0.IMASK1.R = 0xFFFF0000UL;
 
 /* Clear interrupt flags with ones */
 FLEXCAN_0.IFLAG1.R = 0xFFFFFFFUL;
 
 /* Synchronize to CAN bus */
 FLEXCAN_0.MCR.B.HALT = 0U;

Transmit section:

/* clear IRQ flags with ones */
 FLEXCAN_0.IFLAG1.R = 0xFFFFFFFUL;
 
 /* Lock message buffer */
 (void) FLEXCAN_0.MB[0].MB_CS.B.CODE;
 
 /* clear data fields */
 FLEXCAN_0.MB[buffer].MB_DATAL.R = 0U;
 FLEXCAN_0.MB[buffer].MB_DATAH.R = 0U;
 
 /* inactivate buffer */
 FLEXCAN_0.MB[buffer].MB_CS.B.CODE = 0b1000;
 
 FLEXCAN_0.MB[buffer].MB_ID.R = frame->id << 18U;
 
 /* Fill in data...*/
 
 FLEXCAN_0.MB[buffer].MB_CS.B.LENGTH = frame->dlc;
 FLEXCAN_0.MB[buffer].MB_CS.B.IDE = 0U; /* standard id */
 FLEXCAN_0.MB[buffer].MB_CS.B.RTR = 0U; /* data frame */
 FLEXCAN_0.MB[buffer].MB_CS.B.SRR = 0U;
 
 /* start transmission */
 FLEXCAN_0.MB[buffer].MB_CS.B.CODE = 0b1100;

EDIT:

I am getting directly after transmit with "buffer" set to a TXD buffer this signal on the bus:

0690X00000DBntYQAT.png

0690X00000DBntxQAD.png

0690X00000DBnu7QAD.png

(obviously CANoe is sending error frames)

I discovered when I do a non fitting initialization of message boxes but with a number less than the MAXMB value then I get this signal instantly after FLEXCAN_0.MCR.B.FRZ = 0U during init.

And I have the same problem with the examples delivered with SPCStudio.

With Loop-back activated there are no problems.

Thank you in advance!

Regards

Ben

    This topic has been closed for replies.

    1 reply

    DCARR
    Visitor II
    Mar 21, 2022 11:45 AM UTC

    Hi,

    I think that there is a problem in pads configuration.

    Please configure the right RX and TX pads as showed in the below example:

       

      /* Setup FlexCAN 0 pins */

      /* TX (PB0)

        PA = 1 (AF1) / OBE = 1 / ODE = 1 / WPE = WPS = SRC (min value) = 0 */

      SIU.PCR[16].R = 0x0620;

      /* RX (PB1)     IBE = 1 */

      SIU.PCR[17].B.IBE = 0x1;   

    Best regards

    Domenico