Skip to main content
Associate
Jan 8, 2025 10:30 AM UTC
Question

SPC56EL54 - RESET pin is always  pulled down by the CPU

Hi
On power up the SPC56EL54L5CBFS looks like it is in an internal RESET mode that does not  end. 
The RESET pin is always  pulled down by the CPU. 
Power up of 1.2v and 3.3v in 1.5msec.
 
Can you help to to understand why the RESET pin is always  pulled down by the CPU?
 
Thank you.
This topic has been closed for replies.

5 replies

Peter BENSCH
ST Technical Moderator
Jan 8, 2025 11:43 AM UTC

Welcome @GabiPaz-GSP, to the community!

The RESET pin has an internal pull-down. What have you connected externally to the RESET pin?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Jan 8, 2025 12:51 PM UTC

Hi Peter

Thank you, hope that you can help.

1K as pull-up and 10nF  to GND.

The 1.2v and 3.3v provided with 2 DC/DC converters.

 

Peter BENSCH
ST Technical Moderator
Jan 8, 2025 1:22 PM UTC

OK, at least externally RESET is obviously wired correctly.

However, RESET is a bidirectional pin whose internal open drain can be activated by various internal sources. As no information on software etc. is currently available, nobody can make a statement.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Jan 8, 2025 2:43 PM UTC

Hi Peter 

After some testing,

 Internal RESET released after  Power up sequence.   
The Power up sequence should be as following:  3.3V , 1.2v PLL , delay : +500uS - 1.2v Core 
Can you please advice if this  Power up sequence OK?
Gabi
Peter BENSCH
ST Technical Moderator
Jan 8, 2025 3:41 PM UTC

As far as I know, the order does not play a role during power up, you can also switch them on simultaneously.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.