Skip to main content
Matthew Richardson
Associate III
Mar 23, 2018 8:21 AM UTC
Question

SPC56EL Watchdog Timer Interrupt (IVOR12) triggering, but WDT not enabled?

Posted on March 23, 2018 at 09:21

I don't think I have a timer enabled.  I don't see the WDT setting in the outline, but in the configuration.xml it is disabled.  Most importantly clock_cfg.h is  generated as '#define SPC5_DISABLE_WATCHDOG               TRUE'.

However, almost randomly, I am getting an IVOR12 interrupt:

PC 0x00000380

CR 0x44000004

LR 0x00002D78

CTR 0x0

That said, the system runs for ten minutes, one minute, or five, then hangs up in IVOR12.  The only driver I am using is the serial drivers, and may there is an issue there?  It even triggers the ivor when degugging, which I thought the WDT was disabled for debugging as well.  

    This topic has been closed for replies.

    4 replies

    Erwan YVIN
    ST Technical Moderator
    Mar 23, 2018 8:56 AM UTC
    Posted on March 23, 2018 at 09:56

    Hello Matthew ,

    The watchdog is disabled on SWT IP but not in e200 Core (HW WD)

    #if SPC5_DISABLE_WATCHDOG
     /* SWT disabled.*/
     SWT.SR.R = 0xC520;
     SWT.SR.R = 0xD928;
     SWT.CR.R = 0xFF00000AU;
    #endif
    �?�?�?�?�?�?

    About IVOR12,

    the HW Watchdog is enabled by mtMSR (cf boot.s)

    /*
     * MSR default settings.
     */
    #define MSR_DEFAULT (MSR_SPE | MSR_WE | MSR_CE | MSR_ME)
    �?�?�?�?�?

    (cf chapter e200z4 document)

    0690X0000060A0GQAU.png

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Matthew Richardson
    Associate III
    Mar 25, 2018 8:33 AM UTC
    Posted on March 25, 2018 at 08:33

    This one took me a while to troubleshoot.  The unit will literally run for hours without crashing, then sometimes only five minutes and crash without changing any code.  

    I think the issue has something to do with serial_dll.  Our program has a PIT that runs at 50Hz.  The PIT handler is used as an interrupt that periodically loads data onto an RS-232 port.  I've boiled down a program that runs, verse one that eventually crashes.

    NOTE: I feel like this is *not* a IVOR12 issue, as sometimes the IVOR4 and IVOR1 are

    triggered.  I think this issue is related to interrupts, most notably -

    osalEnterCritical(); which is called in sd_lld_write();

    This program crashes periodically (very simplified version for investigation purposes):

    <<<

    int main(void)

    {

       componentsInit();

       irqIsrEnable();

       sd_lld_start(&SD1, NULL);  // baud 19277

       pit_lld_start(&PITD, pit_config);  // 50Hz

       pit_lld_channel_start(&PITD, 2U);

       for ( ; ; )

       {

       }

    }

    uint8_t message[]= 'Hello World!\r\n';

    // PIT

    @

    50Hz 

    void low_speed_PIT(void)

    {

      

    sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0])));

    }

    >>>

    This program runs perfectly

    (note that sd_lld is not called within PIT):

    <<<

    int main(void)

    {

       componentsInit();

       irqIsrEnable();

       sd_lld_start(&SD1, NULL);

    // baud 

    19277

       for ( ; ; )

       {

          sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0])));

          osalThreadDelayMilliseconds(19);

       }

    }

    >>>

    The issue seems (not obviously) related to putting serial data inside a PIT.  I am guessing that this is a

    priority issue.  Is this an uncommon practice?  I think it is corrupting the interrupt scheme somehow.

    Cheers, 

    ~Matt

    Erwan YVIN
    ST Technical Moderator
    Mar 27, 2018 10:26 AM UTC
    Posted on March 27, 2018 at 10:26

    Hello Matthew ,

    According to your description,

    Your issue seems to be a coredump issue or a stack overflow issue.

    A stack overflow could generate a watchdog or a memory corruption

    could you check the state of your stack (cf memory windows) during the IVOR1 ?

    it should be located between __process_stack_base__ and __process_stack_end__

    .core0_stacks : ALIGN(16) SUBALIGN(16)
     {
     . = ALIGN(8);
     __irq_stack_base__ = .;
     . += __irq_stack_size__;
     . = ALIGN(8);
     __irq_stack_end__ = .;
     __process_stack_base__ = .;
     __main_thread_stack_base__ = .;
     . += __process_stack_size__;
     . = ALIGN(8);
     __process_stack_end__ = .;
     __main_thread_stack_end__ = .;
     } > ram�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    Could you increase the Core 0 Process Stack size in order to check the issue is happennign again ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.