Skip to main content
Patriks
Senior
May 13, 2015 8:58 AM UTC
Solved

SPC56EL - using FlexPWM DMA functionality

Posted on May 13, 2015 at 10:58

Hello,

I would like to reload PWM duty cycle every 10 PWM periods using DMA functionality. Therefore I configured FlexPWM subodule 0 and DMA channel An array stores 8 different values for VAL3 register which equal duty cycles from 10%...80%.

My DMA channel step looks like that:

DMAMUX.CHCONFIG[10].R = DMA_CHANNEL_ENABLED | DMA_CHANNEL_NTRIGGERED | 12;

edmaChannelSetup(10,&dcPWM[0],&mcPWM_A.

SUBMOD

[0].

VAL_3

.

R

,2,0,1,1,2,8,-16,0,0);

Now VAL_3 register is written by DMA, but always with the last table element. If I reduce the DMA iterations to 4, then VAL_3 always gets the value of 4th element from my table.I already used DMA for reloading eTimer compare values and had no problems with writing one element from a table to compare registers with each compare event.

Is thereno way to use the next element from table with every reload event? Additionally, I am not quitesure if I understand the reload feature with DMA. The DMAEN register include the VALDE bit. In the reference manual, the description says ''This read/write bit enables DMA write requests for the VALx register when RF is set''. Does it mean that I get one request per VAL register (means totally six) or should the request be used to write all VAL registers with one DMA channel? Best regards, Patrik
    This topic has been closed for replies.
    dangelo.giuseppe-sst
    Visitor II
    Sep 30, 2015 9:09 AM UTC
    Posted on September 30, 2015 at 11:09

    Hello Patrick,

    an external signal can be connected to the FlexPWM EXT_FORCE input using the eTimer_0.CH1 in PULSE-OUTPUT Mode. If the counter is setup for CNTMODE = 001, with the OFLAG OUTMODE set to ‘11111’ (gated clock output) and the ONCE bit not set, the counter will output a pulse stream of pulses that has the same frequency of the selected clock source. The selected clock source can be an external signal, for example, on the eTimer_0.CH0 which is used as input for eTimer_0.CH1.

    Best regards,

    Giuseppe

    5 replies

    Patriks
    PatriksAuthor
    Senior
    May 18, 2015 6:37 AM UTC
    Posted on May 18, 2015 at 08:37

    Hello,

    Two additional questions regarding my issue: 

        - Do I have to set the LDOK bit manually if I update VALx registers with DMA?

        - What about the EXT_FORCE signal? I didn´t find a pin with that function.

    Best regards,

    Patrik
    Erwan YVIN
    ST Technical Moderator
    May 28, 2015 1:06 PM UTC
    Posted on May 28, 2015 at 15:06 Hello Patrik , You are usingenhanced direct memory access(eDMA) with DMA Channel enabled

    with triggering

    . 1) According to the RM ''• 16 independently selectable DMA channels routers – the first 4 channels additionally provide a trigger functionality'' You have to use the first 4 channels 2) i do not see any allocation of edma Channel (edmaChannelAllocate)

    /**
    * @brief EDMA channel allocation.
    *
    * @param[in] ccfg channel configuration
    * @return The channel number.
    * @retval EDMA_ERROR if the channel cannot be allocated.
    *
    * @special
    */
    edma_channel_t edmaChannelAllocate(

    const

    edma_channel_config_t *ccfg) {
     /* If the channel is already taken then an error is returned.*/
     if (channels[ccfg->dma_channel] != NULL)
     return EDMA_ERROR; /* Already taken. */
    
    #if SPC5_EDMA_HAS_MU
    X /* Programming the MUX.(DMA Channel enabled with triggering)*/
     SPC5_DMAMUX.CHCONFIG[ccfg->dma_channel].R = (uint8_t)(0x80 |
     ccfg->dma_periph);
    #endif /* !SPC5_EDMA_HAS_MUX */
    

    3) The reload feature should be triggered by PIT. To set DMAEN is not sufficient. At the end you should launch edmaChannelStart it updates , DMA Set Enable Request Register. For ADC & DSPI , there are some example how to use eDMA. Patrik , do you have an example of your application ? you can send to me directly your application by email. Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    ST Technical Moderator
    May 28, 2015 1:25 PM UTC
    Posted on May 28, 2015 at 15:25

    Hello Patrik ,

        - Do I have to set the LDOK bit manually if I update VALx registers with DMA?

    yes ...

    1) you have to set CLDOK - Clear Load Okay

    2) update VALx registers , 

    3) force the reload of Registers ValueLDOK - Load OK

        - What about the EXT_FORCE signal? I didn´t find a pin with that function. 

    I am checking with PWM Experts.

     

                  Best regards

                           Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Patriks
    PatriksAuthor
    Senior
    Jun 8, 2015 1:17 PM UTC
    Posted on June 08, 2015 at 15:17

    Hello Erwan,

    Ok, now that point is clear to me. Means that I have to set LDOK manually after changing the VALx registers by DMA.

    Only open question is the EXT_FORCE signal. In reference manual chapter14, CTU interaction on page 285 shows that the EXT_FORCE signal for FlexPWM_0 could be eTimer output channel 1. I already tried this interaction and it works well. But I found no solution to use an external signal for as described in 26.2.5

    Best regards,

    Patrik

    dangelo.giuseppe-sst
    Visitor II
    Sep 30, 2015 9:09 AM UTC
    Posted on September 30, 2015 at 11:09

    Hello Patrick,

    an external signal can be connected to the FlexPWM EXT_FORCE input using the eTimer_0.CH1 in PULSE-OUTPUT Mode. If the counter is setup for CNTMODE = 001, with the OFLAG OUTMODE set to ‘11111’ (gated clock output) and the ONCE bit not set, the counter will output a pulse stream of pulses that has the same frequency of the selected clock source. The selected clock source can be an external signal, for example, on the eTimer_0.CH0 which is used as input for eTimer_0.CH1.

    Best regards,

    Giuseppe