Skip to main content
aurelien23
Associate III
Sep 2, 2015 1:30 PM UTC
Question

SPC564B74 FlexCANs are limited to 32 Mailboxes instead of 64

Posted on September 02, 2015 at 15:30

Hello,

I'm using SPC5Studio V3.6 and SPC564B74. The HAL drivers are limiting FlexCAN mailbox number to 32 but this CPU has 64 MB per FlexCAN.

I can change SPC5_CAN_NUM_RX_MAILBOXES and SPC5_CAN_NUM_TX_MAILBOXES définitions in mcuconf.h but this file seems not to be ''patchable''. It has to be changed manually every time the code is generated.

Fixes is welcome.

Aurélien
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Sep 2, 2015 3:41 PM UTC
    Posted on September 02, 2015 at 17:41

    Hello Aurelien,

    there is well an issue SPC564B74 HAL Drivers component.

    it should be limited to 64 not

    we are correcting the issue.

    in waiting for SPC5Studio 3.7, i advice you to put in patch mode in can_lld.c

    (Cf below)

    /**

    * @brief Number of RX mailboxes.

    */

    #undef SPC5_CAN_NUM_RX_MAILBOXES

    #if !defined(SPC5_CAN_NUM_RX_MAILBOXES) || defined(__DOXYGEN__)

    #define SPC5_CAN_NUM_RX_MAILBOXES YOUR_VALUE

    #endif

    /**

    * @brief Number of TX mailboxes.

    */

    #undef SPC5_CAN_NUM_TX_MAILBOXES

    #if !defined(SPC5_CAN_NUM_TX_MAILBOXES) || defined(__DOXYGEN__)

    #define SPC5_CAN_NUM_TX_MAILBOXES YOUR_VALUE_2

    #endif

    #if (SPC5_CAN_NUM_RX_MAILBOXES < 1) || (SPC5_CAN_NUM_RX_MAILBOXES > 64)

    #error ''invalid number of RX mailboxes''

    #endif

    #if (SPC5_CAN_NUM_TX_MAILBOXES < 1) || (SPC5_CAN_NUM_TX_MAILBOXES > 64)

    #error ''invalid number of TX mailboxes''

    #endif

    #if (SPC5_CAN_NUM_RX_MAILBOXES + SPC5_CAN_NUM_TX_MAILBOXES) > 64

    #error ''invalid amount of RX and TX mailboxes''

    #endif

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.