Skip to main content
armitage.richard
Associate II
Sep 30, 2025 3:41 PM UTC
Question

SPC564A compatibility SPC563M

SPC564A datasheet promises compatability.

Does that mean I can swap out SPC563M with SPC564A.

Set target addresses in firmware, build and install, and all runs hunky dory?

This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Oct 2, 2025 8:12 AM UTC

Hello Richard ,

I recommend to check in SPC5Studio Tools Suite

to converge from SPC563M to SPC64A 

(Set target addresses in firmware, build and install)

I have to take care tour pinmap configuration and the IP Iused 

  Best Regards

                 Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
armitage.richard
Associate II
Oct 2, 2025 9:16 AM UTC

Thank you Erwan.

I am unfamiliar with SPC5Studio Tools Suite, I will have ago.

Datasheet promises "3. Pinout compatible with STMicroelectronics’ SPC563M64 devices." for the LQFP176(3).

"I have to take care tour pinmap configuration and the IP Iused " I must ensure any of the new features will not disturb the pin out assignment for the backwards compatibility.

As an aside odd that; spc564a70l7.pdf, September 2013 Doc ID 18078 Rev 4, is still "This is preliminary information on a new product now in development or undergoing evaluation. Details are subject to change without notice."

And imperial air flow 200ft/min ~ 1m/s I guess if you are a 2nd source that happens. Or more likely strict following of JEDEC JESD51-3 from the late 90s. Lets not miss Mars!

Unless there is more guidance lets close.