Skip to main content
Peter Vlna
Associate
June 11, 2018
Question

SPC560P60 after POR no ram init

Posted on June 11, 2018 at 10:33

Hello,

I have encountered problem with my SPC560P60. After power on reset I am stuck at ram init function waiting for POR flag in RGM. My SW distinguish between reset sources and if it is POR I am initializing SRAM.

But in this case I am doing POR and cannot see the corresponding flags after POR and my SW get stuck and reset by SWT.

Peter

#reset #spc56xp60 #rgm
This topic has been closed for replies.

3 replies

Erwan YVIN
ST Technical Moderator
June 12, 2018
Posted on June 12, 2018 at 09:46

Hello Peter ,

Did you try to reset FES and DES ?

https://community.st.com/0D50X00009XkWgeSAF

Best regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Peter Vlna
Associate
June 12, 2018
Posted on June 12, 2018 at 21:54

Hi,

ehm, as I have wrote I am analyzing reset sources and if it was POR I am initializing RAM.

If I erase FES and DES what advantage this brings to me?

I know there was POR, as I did power on board, but your micro isn't reporting that in DES.

And therefore my SW crash as I have no RAM initialized.

Peter

Erwan YVIN
ST Technical Moderator
June 13, 2018
Posted on June 13, 2018 at 11:23

Hello Peter ,

Could you check the others flags ?

'The F_POR flag is automatically cleared on a 1.2 V low-voltage detected or a 2.7 V lowvoltage

detected. This means that if the power-up sequence is not monotonic (i.e., the

voltage rises and then drops enough to trigger a low-voltage detection), the F_POR flag

may not be set but instead the <register>F_LVD12 or <register>F_LVD27_VREG flag is set

on exiting the reset sequence. Therefore, if the F_POR, <register>F_LVD12 or

<register>F_LVD27_VREG flags are set on reset exit, software should interpret the reset

cause as power-on.'

           Best regards

                              Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.