Skip to main content
Marcell Daniel
Associate II
Jul 12, 2017 8:30 AM UTC
Solved

SPC560P ADC value not updating

Posted on July 12, 2017 at 10:30

Hello,

I am workin on SPC560P Discovery Board. I am trying to initialize the ADCperipheral using the components provided in the SPC5 Studio. What I am trying to do is to replicate the ADC Test Application in a different project. I initialize the ADC component in the project configuration andusing this in the main.c

#include 'components.h'
#include 'adc_lld_cfg.h'
static adcsample_t samples[ADC1_GROUP_ADC1_CONF_NUM_CHANNELS *
 ADC1_GROUP_ADC1_CONF_BUF_DEPTH];
static uint32_t mswaittime;

int main(void) {
 componentsInit();
 irqIsrEnable();
 adc_lld_start(&ADCD2, NULL);
 sysWaitMilliseconds(1000UL);
 while(1) { 
 adc_lld_start_conversion(&ADCD2, &adc1_group_ADC1_conf,
 samples, ADC1_GROUP_ADC1_CONF_BUF_DEPTH);
 mswaittime = samples[0];
 sysWaitMilliseconds(100UL+mswaittime);�?�?�?�?�?�?
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Configuring the ADC I am using the same values provided in the ADC Test Application (channel: 10).

The problem is after loading the program on the board, that the ADC sample values are not updating, but remaining on a constant value. Removing the jp12 jumper is setting the sample value to 1, but changing the resistor has no effect on the sample value.

Can you help me out what am I missing here?

Regards,

Marcell

#spc560p #adc #spc5studio #udetsk
This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Jul 13, 2017 3:33 PM UTC
Posted on July 13, 2017 at 17:33

Hello Marcell ,

Warning : for Standard channel , we should PSAMP to 50 

Have you configured correctly your pinmap Wizard ?

0690X00000607aZQAQ.png

Did you arrive to End Of Conversion Interrupt ?

   Best Regards

         Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Jul 13, 2017 3:33 PM UTC
Posted on July 13, 2017 at 17:33

Hello Marcell ,

Warning : for Standard channel , we should PSAMP to 50 

Have you configured correctly your pinmap Wizard ?

0690X00000607aZQAQ.png

Did you arrive to End Of Conversion Interrupt ?

   Best Regards

         Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Marcell Daniel
Associate II
Jul 14, 2017 9:36 AM UTC
Posted on July 14, 2017 at 09:36

Thanks Erwan!

Somehow I forgot the Pinmap Wizard again, now it is works as expected. 

While I am here may i ask about the FlexRay driver? I found many thread here asking about the Flexray driver and I understand that SPC5 studio is not containing support for Flexray, nor it is planned in the near future. However you wrote that the driver is available in the SPC5 MCAL package which can be download under this

https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/spc5-embedded-software/stsw-spc56as003.license%3d1499936172099.html

. This page contains a Request Software. I filled the form out and requested the software and now it says its under Validating. 

Edit: I was finally able to download the Autosar 4 MCAL package. I submitted my license request to 

mailto:apgtools-license@st.com

 for a Demo version. I am waiting for the Serial Number so i can install the package.

Thanks for helping me!

Regards,

    Marcell