Skip to main content
ssk
Associate III
Jun 30, 2015 2:50 PM UTC
Question

SPC560D - power control modes

Posted on June 30, 2015 at 16:50

Hello,

I am using standby mode for SPC560D MCU. The datasheet mentions about using DRUN or software reset for exiting this mode. Can you please explain on,

1. How to configure the DRUN mode? I tried using API 'halSPCSetRunMode' for switching between modes. But when used for DRUN mode, it does not exit the standby mode correctly and a power reset is required. Is any thing missing for this?

2. Which are the ways to use software reset for SPC560D? Can I use watchdog reset as a software reset? Is there any other means for software reset?

Thanks in advance for any help.

Mike.
    This topic has been closed for replies.

    61 replies

    nooshin_1382
    Associate III
    Oct 15, 2015 10:44 AM UTC
    Posted on October 15, 2015 at 12:44

    Hello Erwan

    Thanks so much for your help in this issue to me.

    I test the code in my application it ok for me but have some RESET issue when wakeup from RAM .

    is exist any way to save the flash address and when wakeup from ram jump to this address?

    Best Regards

    Nazerian Vanima

    Erwan YVIN
    ST Technical Moderator
    Oct 15, 2015 3:09 PM UTC
    Posted on October 15, 2015 at 17:09

    Hello Vanima ,

    Could you send me your full application not only the main.c file ? if there is some company restricted code you can send directly by email anyway could you relocate the code halSPCSetRunMode in RAM ? like below :

    _attribute__ ((section (
    ''.codeinram''
    ))) 
    void
    gotoStandbyMode(
    void
    ) {
    WKUP.WISR.R = 0x00000008; 
    //Clear interrupt flag
    if
    ((ME.GS.B.CURRENTMODE < SPC5_RUNMODE_RUN3)
    || (ME.GS.B.CURRENTMODE > SPC5_RUNMODE_RUN0)) {
    /* Clearing status register bits I_IMODE(4) and I_IMTC(1).*/
    ME.IS.R = 5;
    /* Starts a transition process.*/
    ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_STANDBY) | SPC5_ME_MCTL_KEY;
    ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_STANDBY) | SPC5_ME_MCTL_KEY_INV;
    /* Waits for the mode switch or an error condition.*/
    while
    (TRUE) {
    } 
    }
    }
    __attribute__ ((section (
    ''.codeinram''
    ))) 
    void
    gotoRunMode(
    void
    )
    {
    /* Clearing status register bits I_IMODE(4) and I_IMTC(1).*/
    ME.IS.R = 5;
    /* Starts a transition process.*/
    ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_DRUN) | SPC5_ME_MCTL_KEY;
    ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_RUNMODE_DRUN) | SPC5_ME_MCTL_KEY_INV;
    /* Waits for the mode switch or an error condition.*/
    while
    (TRUE) {
    } 
    }

    there is an important thing. if a WAKEUP Event is pending, you can not enter in Sleep Mode (STANDBY). Best Regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    nooshin_1382
    Associate III
    Oct 27, 2015 9:14 AM UTC
    Posted on October 27, 2015 at 10:14

    Hi Erwan

    Sorry For my late answer.

    I test this code but MCU is reset when the wakeup signal is generated.

    I use this mode permanently for my project i should save my parameters status in Virtual eeprom.

    i don't know what happen for this mode.

    i send my test project for you this project have the same response on my real project.

    thanks so much For your kind attention Erwan.

    Best Regards

    Nazerian Vanima

    ________________

    Attachments :

    Led_Blinker.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0TZ&d=%2Fa%2F0X0000000bZP%2F4PqXUNXUncH4B3LhBZuYd8YTlaAXTlMG7_ax0B14jFA&asPdf=false
    nooshin_1382
    Associate III
    Oct 27, 2015 12:18 PM UTC
    Posted on October 27, 2015 at 13:18

    Hi Erwan

    I send You an email for this issue .

    this is an example for standby mode enter and exit .

    Best Regards

    Nazerian Vanima

    philipp239955_stm1_stmicro
    Associate II
    Nov 17, 2015 8:13 AM UTC
    Posted on November 17, 2015 at 09:13

    Hi Community

    I have some trouble with the reset after wakeup. I try to enter Run from Standby. During this mode transition, the microcontroller gets a reset and the data in the SRAM are lost. Functions were stored in the .codeinram section and the Boot from BKUPRAM FLAG is active.

    Is there a solution for this?

    kind regards

    Philipp

    Erwan YVIN
    ST Technical Moderator
    Nov 17, 2015 9:46 AM UTC
    Posted on November 17, 2015 at 10:46

    Hello Philipp ,

    Did you use PLS Debugger ?

    In our configuration , by Default , Hardware Reset Mode is set.

    could you disable this mode please and retest ?

    (cf cfg file in UDE directory)

    Use Hardware Reset Mode

    When this option is enabled the normal mechanism setting the startup program counter to the start symbol of the loaded program by the debugger is disabled. There are two modes selectable:

    (the 2 modes are not selectable in PLS 4.02+ with SPC57 patches)

    • Simulate boot code: The flash is searched for a valid reset configuration halfword (RCHW). If a valid word is found, the address is read from the correct and used as the start address. The behavior is similar to the BAM flow during power on reset.

    • Execute boot code: The PC is set to the entry point of the bootcode if there is boot code available

    This option is especially helpful if programs are debugged where an additional loader program is already flashed into the target. That option is also needful to check, if the application starts correctly when the debugger is not connected.

    Be aware that if the target processor is not correctly configured, e.g. there is no boot code or buggy bootcode, using the Hardware Reset Mode can result in unpredictable behavior.

    Load in Ram issue with PLS will be solved in SPC5Studio 4.0.

          Best Regards

                    

                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    philipp239955_stm1_stmicro
    Associate II
    Nov 17, 2015 11:27 AM UTC
    Posted on November 17, 2015 at 12:27

    Hi Erwan

    Thank you for your fast reply. Yes I’m using the PLS integrated Debugger, which is delivered on board.

    The Hardware Reset Mode is already deselected, but I’m using 4.04 PLS UDE so have no selectable modes.

    I did some changes in my application. Boot from BKUP Ram is disabled. I need for my application some data in the SRAM, which should be still valid after wake up. (Boot from BKUP RAM is not necessary, it was a disaccord from me)

    The new behavior is the behavior before. The microcontroller goes into STANDBY and if the SW2 is pressed it wakes up. During the wakeup process the microcontroller get a reset. The stored data in the SRAM corrupt through this reset. The difference to the behavior before is that the reset doesn’t occur during debugging with PLS. It only occurs if the UDE platform is closed and application is running without the debugger.

    Is there another solution to store data before the reader goes into STANDBY? (Data Flash has not enough write cycles. The configuration/timings must be stored on very switch into standby).

    Used Hardware: SPC560D Discovery Board

    kind regards

    Philipp

    Erwan YVIN
    ST Technical Moderator
    Nov 25, 2015 9:04 AM UTC
    Posted on November 25, 2015 at 10:04

    Hello Philip,

    Please use PLS 4.02, this version is more stable

    According to the RM, (D Bolero)

    the first 8K SRAM could be still ON.

    ''The only parts of the device that are still powered during this mode are pads

    mapped on wakeup lines and power domain #0 which contains the MC_RGM, MC_PCU,

    WKPU, 8K RAM, RTC_API, SIRC, FIRC, and device and user option bits.''

    Warning , after STANDBY entry, the debugger loses connection to the target due to

    power gating.

        Best regards

                            Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    ST Technical Moderator
    Nov 25, 2015 4:14 PM UTC
    Posted on November 25, 2015 at 17:14

    Philipp ,

    Full answer in [DEAD LINK /public/STe2ecommunities/mcu/Lists/SPC56/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/SPC56/Using%20SRAM&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C7B65FFB6DB42540A4DAECE852348058&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/SPC56/AllItems.aspx&currentviews=49]https://my.st.com/public/STe2ecommunities/mcu/Lists/SPC56/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSPC56%2fUsing%20SRAM&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C7B65FFB6DB42540A4DAECE852348058&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSPC56%2FAllItems.aspx&currentviews=49

      Best regards

                      Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    philipp239955_stm1_stmicro
    Associate II
    Nov 27, 2015 12:17 PM UTC
    Posted on November 27, 2015 at 13:17

    Hi Erwan,

    Thank you for your reply. I hope the SRAM Testapplication will included in the next SPC5 Studio Release.

    The reset behvoir during the wakeup phase is not explainable for me. I figured out that the Software Watchdog Reset Flag (RGM.DES.B.F_SWT) is active after Wakeup. Some time the Reset Flags are External Reset and SWT_Reset after wakeup or only SWT reset.

    Has anyone an explanation for this strange behavior?

    Some Information:

    GotoStandby:

    WKUP.

    WISR

    .

    R

    = 0x00000008;                                          

    //Clear interrupt flag

     

    if

    ((ME.

    GS

    .

    B

    .

    S_CURRENTMODE

    <

    SPC5_RUNMODE_RUN3

    ) || (ME.

    GS

    .

    B

    .

    S_CURRENTMODE

    >

    SPC5_RUNMODE_RUN0

    )) {

        ME.

    IS

    .

    R

    = 5;                                                     

    // Clearing status register bits I_IMODE(4) and I_IMTC(1).

       

    /* Starts a transition process.*/

        ME.

    MCTL

    .

    R

    = SPC5_ME_MCTL_MODE(

    SPC5_RUNMODE_STANDBY

    ) | SPC5_ME_MCTL_KEY;

        ME.

    MCTL

    .

    R

    = SPC5_ME_MCTL_MODE(

    SPC5_RUNMODE_STANDBY

    ) | SPC5_ME_MCTL_KEY_INV;

       

    /* Waits for the mode switch or an error condition.*/

       

    while

    (TRUE) {

          uint32_t r = ME.

    IS

    .

    R

    ;

         

    if

    (r & 1)

           

    break

    ;

         

    if

    (r & 4)

           

    break

    ;

        }

    GotoRun:

    OSAL_IRQ_HANDLER(vector46) {

      uint32_t wisr;

      OSAL_IRQ_PROLOGUE();

      wisr = WKUP.

    WISR

    .

    R

    ;

      WKUP.

    WISR

    .

    R

    = wisr;

      ME.

    IS

    .

    R

    = 5;

      ME.

    MCTL

    .

    R

    = SPC5_ME_MCTL_MODE(

    SPC5_RUNMODE_DRUN

    ) | SPC5_ME_MCTL_KEY;

      ME.

    MCTL

    .

    R

    = SPC5_ME_MCTL_MODE(

    SPC5_RUNMODE_DRUN

    ) | SPC5_ME_MCTL_KEY_INV;

     

    while

    (TRUE) {

        uint32_t r = ME.

    IS

    .

    R

    ;

      

    if

    (r & 1)

        

    break

    ;

      

    if

    (r & 4)

        

    break

    ;

      }

      OSAL_IRQ_EPILOGUE();

    }

    I tested it with the debugger and without the debugger. So there is the same behavior.

    kind regards

    Philipp