Skip to main content
philipp239955_stm1_stmicro
Associate II
Apr 5, 2016 11:16 AM UTC
Question

SPC560D Power consumption

Posted on April 05, 2016 at 13:16

Hi Community

I have some issues/questions about the power consumption of the SPC560D40L1 CPU.

 I found this document on the ST-Website

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/CD00291326.pdf

There the STANDBY mode is described with max. 300µA and min with 21µA.

Is it possible to reach the 21µA power consumption, without an external Oscillator, because I cannot find any register to enable the 128khz oscillator as system clock during STANDBY mode? I mean if I disable the FIRC the CPU has no clock anymore?

Kind regards

Philipp

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Apr 19, 2016 7:28 AM UTC
    Posted on April 19, 2016 at 09:28

    Hello Philipp ,

    Sorry for the late answer ,

    there are 2 registers :

    SIRC_CTL with bit SIRCON_STDBY to disable SIRC in STANDBY MODE

    SIRCON_STDBY 

    SIRC control in STANDBY mode.

    0 SIRC is switched off in STANDBY mode.

    1 SIRC is switched on in STANDBY mode.

    FIRC_CTL with bit FIRCON_STDBY to disable FIRC 

    FIRCON_STDBY

    FIRC control in STANDBY mode.

    0 FIRC is switched off in STANDBY mode.

    1 FIRC is in STANDBY mode.

    There is no clock anymore ..

    you need to use a WAKEUP Interrupt to go out from STANDBY mode.

           Best regards

                 Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    philipp239955_stm1_stmicro
    Associate II
    Apr 22, 2016 6:41 AM UTC
    Posted on April 22, 2016 at 08:41

    Hi Erwan, 

    Thanks for your reply. Yes the missing information for me was that the CPU does not need a clock source during STANDBY. However thank you for your reply. Now i can reach the 30µA Standby current. 

    kind regards

    Philipp