Skip to main content
AndreasPA
Associate III
Oct 15, 2020 12:55 AM UTC
Solved

SPC560D CAN baudrate confirmation

Hello all,

im working on a project that uses an SBC, using my logic analyser i can confirm data is coming and and looks to be a can signal but it seems my baud rate timing is incorrect or something else is amiss.

my board is the SPC560DL1, i understand the the flexcan uses Perphial set 2 clock so mine by default is set to 24Mhz.

0693W000004JohiQAC.pngi've attached images of my settings and results

http://www.bittiming.can-wiki.info/#Freescale

here is the table i've created with < 24Mhz, 75% sample point >

0693W000004Joi2QAC.png 

my settings for 250 are

sample point @ 75%, i've also tried 87.5

Pclk 24Mhz

propseg= 2

pseg1 =7

pseg2 =3

presdiv =6

which should solve to 24,000,000/6 = 4000000

4000000/16 = 250 baud

0693W000004Joh9QAC.png0693W000004JohEQAS.png 

Here is my code snippit that i'm using to test can functionality

0693W000004JohnQAC.pngdata on my output looks like this

0693W000004JojjQAC.pngwith my analyer it's seeing garbage on the decoder side so im guessing the timing is incorrect

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Nov 19, 2020 9:00 AM UTC

    0693W000005BvCaQAK.pngHello,

    the issue is in your configuration.

    the formula to calculate the clock is:

    PCLK / (PRESDIV + 1)

    So, in your configuration PRESDIV has to be set to 5 (and not to 6)

    Regards,

    Giuseppe

    7 replies

    Erwan YVIN
    ST Technical Moderator
    Oct 16, 2020 8:38 AM UTC

    Hello ,

    According to your settings ,

    the bitrate should be 250 Kbit/s

    I do not see any timing or scale in your screenshot ...

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    AndreasPA
    AndreasPAAuthor
    Associate III
    Oct 21, 2020 2:58 AM UTC

    Hey Erwan, i found out that beyond 20kbps the can signal becomes unstable.

    i was told that i should be using the external clock to which i've tried enabling but when i do it results in a system reset.

    is there a process to enabling the external clock ?

    these also some boxes like enable clockout that i dont quite understand what it exactly does.

    a guess would be that you would need to tick it along with the bypass clock but in doing that i still get an unexpected reset.

    0693W000004KT4IQAW.png 

    on my board i have the the CSTNE16M0V53C000R0 (16Mhz) which is advertised to be an alternative to the one used in the spc560d disc board.

    AndreasPA
    AndreasPAAuthor
    Associate III
    Oct 18, 2020 11:11 PM UTC

    Hey Erwan,

    here is an attached image, the data constantly changes along with everything else but here is one that had more data than the rest and with a timing marker as well.

    Setup:

    0693W000004KAlrQAG.pngThe actual id is 0x70

    8 bytes of data where the message is 0F 00 00 00 00 00 00 0F

    I've also attached the file with the entire can recording ( program is logic 2 from salaeae) , also added in the timing for the start and end.

    0693W000004KAlwQAG.png 

    AndreasPA
    AndreasPAAuthor
    Associate III
    Oct 18, 2020 11:16 PM UTC

    0693W000004KAmpQAG.pngattached image of setup code, adjusted since the original post

    AndreasPA
    AndreasPAAuthor
    Associate III
    Oct 18, 2020 11:54 PM UTC

    Here is also a setup using the mcp2551 with just 2 120 ohm resistors at each end

    the data in this message should be different to the prior as this is on my spc560d-dis board

    channel 2 and 3 are connected to TX and RX

    0693W000004KAsTQAW.pngEdit: had accidently marked vdd to be gnd0693W000004KKAHQA4.png

    Giuseppe DI-GIORE
    ST Employee
    Nov 19, 2020 9:00 AM UTC

    0693W000005BvCaQAK.pngHello,

    the issue is in your configuration.

    the formula to calculate the clock is:

    PCLK / (PRESDIV + 1)

    So, in your configuration PRESDIV has to be set to 5 (and not to 6)

    Regards,

    Giuseppe

    AndreasPA
    AndreasPAAuthor
    Associate III
    Nov 20, 2020 2:28 AM UTC

    You are a livesaver!

    To avoid this issue for anyone else, would it be possible to change or add in a note to the application configuration page ?

    0693W000005C3KSQA0.png