Skip to main content
ARicc.385
Visitor II
Jun 29, 2020 8:05 AM UTC
Solved

SPC560B60L7 microntroller compatibility with MPC5606B

Hi,

I'm doing a HW rework design about a board that use the microcontroller MPC5606B of NXP. I want update the design using a ST microcontroller. I have seen that this device is similar to the SPC560B60L7, but I would like to know if the 2 IC are pin-to-pin compatible. In particular, is it possible to replace one component with the other one without modify the electrical connections already present on the board?

The complete part number identified are: SPC5606BF1VLU6 (of NXP) and SPC560B64L7C6E0X (of ST).

Thank you,

Regards.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 2, 2020 8:34 AM UTC

    Honestly , it is the same IP for SPC560 and MPC560.

    the part number are different.

    B64 means 1.5 MB Flash

    L7 LQFP176 Pins

    I recommend to use the 2 pinmap editors (1 from SPC5Studio and 1 from NXP May be S32 Design Studio)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 2, 2020 8:34 AM UTC

    Honestly , it is the same IP for SPC560 and MPC560.

    the part number are different.

    B64 means 1.5 MB Flash

    L7 LQFP176 Pins

    I recommend to use the 2 pinmap editors (1 from SPC5Studio and 1 from NXP May be S32 Design Studio)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.