Skip to main content
mbahtat
Visitor II
Dec 7, 2015 11:46 AM UTC
Question

SPC560B60, SPC560B64 and ''Freescale SPC5607B'' compatibility

Posted on December 07, 2015 at 12:46

Good morning,

I've 2 questions:

First, I'm wandering about the differences between: the SPS560B60 and the SPS560B64? Are they compatible in the sense that the same code would run the same in both devices? (I'm already aware of FLASH/RAM memory sizes difference, is there any other difference?).

Second, how much compatible a code that was running into the ''Freescale SPS5607B'', would run into the ''ST SPS560B60'' ?

Many Thanks.

Kind Regards.

#spc560-mcu
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Dec 7, 2015 1:34 PM UTC
    Posted on December 07, 2015 at 14:34

    Hello ,

    the difference is just the flash size.

    1M (for 60) 1.5MB for 64

    you can use the same code.

    you have to just to check your mapping LQFP100 / LQFP144

    the code ''Freescale SPS5607B'' (1.5 MB) is compliant for B60 and B64.

    it is the same device.

        Best regards

                    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.