Skip to main content
VOtev
Visitor II
Jan 4, 2019 1:40 PM UTC
Solved

SPC560B50L3, Cannot use eMIOS0 ch1-ch7 as PWM outputs?

Hi ST experts,

I started with SPC560B50L3 and I am using SPC5Studio 5.8. I have problem with eMIOS0 configuration (ch1-ch7) as PWM outputs.. I use PinMap editor and i configured the pins as eMIOS0 output (eMIOS0 ch1-ch7, eMIOS0 ch9-ch13 and eMIOS0 ch20-ch21).

I can configure eMIOS0_group0 (ch9-ch15) and eMIOS0_group1 (ch17-ch23) but cannot configure eMIOS0 ch1-ch7 as PWM, why?

I saw into RM0017 document on figure 250 channel configuration. How i understand it.. there are 6 PWM output groups.. 3 groups for eMIOS0 and 3 groups for eMIOS1, is not it? For package, which i use, i can used only eMIOS0 (LQFP100) and i need to use all three groups of eMIOS0 for PWM outputs.

But via Low Level Driver configuration, i can configure only two groups of eMIOS0 as PWM output.

I use SPC560B54L5 and i saw in document RM0037 (figure 357) very similar channel configuration as for SPC560B50L3. I used the MCU with SPC560B-DIS board and there is no problem configured all 3 groups of eMIOS0 as PWM output.

Please, can you explain me what i do wrong?

Thank you for help

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Jan 10, 2019 9:59 AM UTC

Hello Vit ,

It is the driver implementation .

You need to update the driver in order to support it.

not to use the component.

Best regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Jan 10, 2019 9:59 AM UTC

Hello Vit ,

It is the driver implementation .

You need to update the driver in order to support it.

not to use the component.

Best regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.