Skip to main content
Visitor II
Jul 10, 2026 5:43 AM UTC
Question

SPC560B50L1 - WKPU/PA4 Wakeup Configuration in SPC5 Studio + Bootloader/FW Update Example Needed

Hi All,

We are developing a BMS application using the SPC560B50L1 microcontroller with SPC5 Studio, and need help with two topics:

1) Low-Power Mode Wakeup via PA4 (WKPU9)

We want to put the SPC560B50L1 into a low-power mode (STOP/STANDBY) and wake it up using pin PA4, which maps to WKPU channel 9 as per the SPC560Bxx Reference Manual (RM0017, Table 96 - Wakeup Vector Mapping).

However, in SPC5 Studio, under "SPC560BCxx Low Level Drivers Component RLA" -> "Enabled Drivers", there is no dedicated WKPU driver option available (unlike some other device families, e.g. SPC582Bxx, which do expose a WKPU checkbox).

Could someone please help with:
- The correct/recommended way to configure WKPU9 (PA4) as a system wakeup source on SPC560B50L1 within SPC5 Studio
- Any example project or reference code demonstrating:
  a) EIRQ/WKPU channel configuration for a specific pin
  b) Enabling system wakeup capability (WRER register or equivalent) so the configured pin can wake the MCU from STOP/STANDBY mode
  c) Any required Mode Entry (ME) module configuration to allow this wakeup source in the target low-power mode

2) Bootloader / Firmware Update Example

Separately, we are planning to implement a firmware upgrade (bootloader) mechanism for this MCU as part of our production rollout. Could someone share:
- Any example bootloader project or reference code for the SPC560B50L1 (or broader SPC560Bxx family)
- Any relevant Application Notes covering bootloader design, in-application programming (IAP), or firmware update strategies for this device

Device details:
- MCU: SPC560B50L1
- Tool: SPC5 Studio
- Driver package: SPC560BCxx Low Level Drivers Component RLA

This is fairly urgent for us as we are on a tight production timeline. Any guidance, example code, or pointers to relevant documentation would be greatly appreciated.

Thanks in advance!
 

Best regards,

Pandiyan T

1 reply

Associate II
Sep 24, 2026 8:43 AM UTC

which one is used?SPC560B50L1 or SPC560BCxx?The SPC5 studio may have limited part number support. The SPC582B may be ok