Skip to main content
AChan.5.20
Associate
Apr 8, 2019 12:02 PM UTC
Question

SPC560B40L3 Analog watchdog for pulse transition period detection.

Hello,

I want to sense period of 4 pulses using Analog Watchdog. I am using SPC560B40L3(100Pin controller). My requirement is to sense the Analog window voltage.

Ex. Square wave Pulse varies from 0.5V to 4.5V. And if I put my thresholds for every pulse on 1V(LOW threshold) & 4V(HIGH threshold). Is it possible to detect individual pulse transition period measurement?

Thanks,

Ashok

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Apr 11, 2019 8:34 AM UTC

    Hello ,

    i think that it is possible

    By using emios ,

    Input Period Measurement (IPM) mode cf RM017

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    AChan.5.20
    Associate
    Apr 12, 2019 4:22 PM UTC

    Thanks for response.

    I think by using IPM I'll be able to measure total pulse not half pulse(High/Low Period) please correct me if I am wrong. By using Analog watch I want to measure half pulse period for multiple channels.