Associate
May 10, 2018 4:58 AM UTC
Question
SPC560B Discovery board , Issue with stop mode .
- 1 reply
- 1039 views
Posted on May 10, 2018 at 06:58
I am using spc560b discovery board , i want to implement low power modes like halt , stop and standby ,
i am able to implement standby mode and waking up with CAN Rx at PB1 , however when i try with stop mode
i think it got hang and current consumption not get reduced and it didn't wakeup like in standby mode .
For sleep i am using PA3 pin interrupt , most of the code i have took from the example project , SPC560Bxx_OS-Less_STANDBY_Test_Application_for_Discovery that i got in different thread .
I am sharing code as attachment any help will be appreciated .
#issue-with-stop-mode-. #spc560b-discovery-board