Skip to main content
jleech92
Visitor II
Apr 13, 2015 9:42 AM UTC
Question

SPC560B-DIS Watchdog Issues

Posted on April 13, 2015 at 11:42

Hello,

I am currently trying to set up the Watchdog on my SPC560B board.

Firstly, after enabling the watchdog and letting it time-out into a reset, it then enters SAFE mode and does not reset the program. RGM.DERD is set to 0 so the watchdog time-out should just reset the program from what I understand?

Also, when trying to use the interrupt-then-reset option, the triggered interrupt generates an SE_ILLEGAL and I'm not sure why that is? I have set up the interrupts correctly from what I can tell, setting them up in a similar way to ones I have previously done.

Any help greatly appreciated, thanks.

#spc560b-watchdog-issues
    This topic has been closed for replies.

    2 replies

    kevin239955_st
    Associate III
    Apr 13, 2015 4:46 PM UTC
    Posted on April 13, 2015 at 18:46

    Hi Jack

    I do know that when I booted the processor from Flash the SWT in its default state would constantly reset the board, until I disabled it using the script in UDE.

    Kevin

    Erwan YVIN
    ST Technical Moderator
    Apr 29, 2015 12:48 PM UTC
    Posted on April 29, 2015 at 14:48

    Hello Jack ,

    Did you solve your issue ? we disable the WD by using the following command

    /* SWT disabled.*/
    SWT.SR.R = 0xC520;
    SWT.SR.R = 0xD928;
    SWT.CR.R = 0xFF00000A;

    if you want to enable it , you have to update your WSC (SR) Watchdog Service Code.This field is used to service the watchdog and to clear the soft lock bit (SWT_CR.SLK). To service the watchdog, the value 0xA602 followed by 0xB480 is written to the WSC field. To clear the soft lock bit (SWT_CR.SLKSWT_CR.), the value 0xC520 followed by 0xD928 is written to the WSC field. and you have to set correctly SWT_CR maybe ITR ITR Interrupt Then Reset. 0 = Generate a reset on a time-out 1 = Generate an interrupt on an initial time-out, reset on a second consecutive time-out (Cf Chapter 35) Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.