Skip to main content
Alok Nigam_2
Associate
Apr 6, 2018 10:20 AM UTC
Question

SPC560B-DIS , watch dog issue in debug mode .

Posted on April 06, 2018 at 12:20

I am using SPC560B-DIS  discovery board and UDE STK 4.8  debugger for my project .

I am facing issue with watchdog during debugging  , i have set my watchdog in window mode

with time out period of 100 ms , and window as 50 ms .

I am not servicing watchdog to check whether watchdog  reset or not after 100 ms , by analyzing one pin state 

in oscilloscope .In oscilloscope i am able to see pin state change for very short time , but differences between consecutive peaks is coming accurately 100 ms . 

I have put FRZ bit as 0 so watchdog  counter will increment in debug mode .

Issue : When i debug the code using 

UDE STK 4.8 , reset is happening and continuous 

warning messages are displaying in log window with time stamps .

But when i am putting the break point in main , it is not hitting frequently but randomly

like sometimes in seconds , sometimes in minutes . 

But warning in message log is displaying very frequently. 

I don't know the cause of this issue , any help will be appreciated for solving this issue .  

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Apr 9, 2018 8:43 AM UTC
    Posted on April 09, 2018 at 10:43

    Hello Alok ,

    If you have a reset issue ramdomly, which IVORx are you going ? 

    Check your LR,PC ..

    For your information , the Watchdog is disable on your debug configuration on your default configuration.

    0690X0000060AU5QAM.png

               Best Regards

                                Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Alok Nigam_2
    Associate
    Apr 10, 2018 8:35 AM UTC
    Posted on April 10, 2018 at 08:35

    Hi erwan , i have removed the watchdog de-init previously . Please see the pic below

    0690X0000060ASUQA2.png

    Here watchdog reset  is happening in 100 ms and i am able to see the warning message ,through

    pin state i have confirmed reset time out is 100 ms , but the break point before TIMT_Start()

    is not hitting after target reset every time , some times it hits the break point and that also with 

    different intervals .