Skip to main content
ssk
Associate III
Aug 12, 2015 1:03 PM UTC
Question

SPC560 - SWT

Posted on August 12, 2015 at 15:03

Hello,

I am using software watchdog timer (SWT) for the SPC560D40 MCU. What is the 'out of reset' situation for the SWT?

Best Regards,

Mike.

#swt
    This topic has been closed for replies.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    Aug 17, 2015 9:44 AM UTC
    Posted on August 17, 2015 at 11:44

    Hello Mike ,

    it depends of your configuration :

    on SWT_CR, there is a bit to set your ''out of reset''

    ITR

    Interrupt Then Reset.

    0 = Generate a reset on a time-out

    1 = Generate an interrupt on an initial time-out, reset on a second consecutive time-out

    Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Aug 18, 2015 8:02 AM UTC
    Posted on August 18, 2015 at 10:02

    As per reference manual, the reset state for ITR is 0 i.e. generate a reset on timeout but What will be the default value used to decide the timeout (before it is initialized to some value)?

    Best Regards,

    Mike.

    Erwan YVIN
    ST Technical Moderator
    Aug 19, 2015 11:58 AM UTC
    Posted on August 19, 2015 at 13:58

    Hello Mike ,

    The default value is 

    Default counter value (SWT_TO_RST) is 1280 (0x00000500 hexadecimal)

    which

    correspond to around 10 ms with a 128 kHz clock.

        Best Regards

                          Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Aug 19, 2015 2:38 PM UTC
    Posted on August 19, 2015 at 16:38

    The default value is considering 128KHz clock but I am using 8MHz external XTAL. In this case what will be the value for timeout at the time of reset?

    Mike.

    Erwan YVIN
    ST Technical Moderator
    Aug 24, 2015 9:21 AM UTC
    Posted on August 24, 2015 at 11:21

    Hello Mike ,

    The unique SWT counter clock is the undivided slow internal RC oscillator 128 kHz

    (SIRC), no other clock source can be selected

       Best Regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.