Skip to main content
ssk
Associate III
Dec 8, 2015 1:24 PM UTC
Question

SPC560 Flash protection

Posted on December 08, 2015 at 14:24

I am using SPC560D MCU along with SPC5Studio. I am using PLS UDE for flash programming and debugging. I want to protect the device flash memory - code and data both from read and writing once final version is programmed. Has anyone tried this? Whether PLS UDE supports such kind of protections?

I read about the Censorship topic (section 5.1.3/ page #75) in reference manual. Can this feature serve my purpose? Has anyone used this? How this works for code and data flash? Can someone explain this elaborately?

Thanks in advance.

Mike
    This topic has been closed for replies.

    6 replies

    Erwan YVIN
    ST Technical Moderator
    Dec 9, 2015 10:53 AM UTC
    Posted on December 09, 2015 at 11:53

    Hello Mike ,

    yes you have to read carrefully the chapter 5.1.3

    you have to update :

    NVPWD0 = 0xFEED_FACE

    NVPWD1 = 0xCAFE_BEEF

    you have to change :

    BootPasswd0=0xFEEDFACE

    BootPasswd1=0xCAFEBEEF

    in cfg file, UDE Directory.

    without the good password, it is not possible to flash.

                Best Regards

                           Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Dec 9, 2015 12:07 PM UTC
    Posted on December 09, 2015 at 13:07

    Thanks Erwan for your reply.

    Can this protect the flash from reading as well as for writing? I want to protect my device from reverse engineering point of view i.e. I want to protect my device from reading the flash and also want to protect for false writing. Can this be achieved using the 'Censorship' feature? Can you please provide more details in this regard? Any app note will be useful.

    Thanks in advance.

    Mike

    Erwan YVIN
    ST Technical Moderator
    Dec 9, 2015 4:26 PM UTC
    Posted on December 09, 2015 at 17:26

    Hello Mike ,

    Did you Flash memory boot ?

    if yes ,

    The best mode for your case is to use the censored mode.

    Private Flash Memory Password and censored

    1) Set NVSCC0(CW) , NVSCC1(CW) different to 0x55AA.

    Set NVSCC0(SC) , NVSCC1(SC) equals 0x55AA.

    IMPORTANT : NVSCC0(CW,SC) must be equal to NVSCC1(CW,SC) otherwise your chip will be completely locked.

    2) Define NVPWD1,NVPWD2- Your 64 bit passwords (keep them secret).

    it will not possible anymore to use PLS UDE except with the good defined password.

    BootPasswd0=NVPWD0 (your pass)

    BootPasswd1=NVPWD1 (your pass)

    Best regards

    Erwan

    ________________

    Attachments :

    2015-12-09_154413.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I02m&d=%2Fa%2F0X0000000bZe%2F4fk_7ytBbK_gTmz7ZjdzplvrR7jIEHYwuOvJNLR9E_g&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Dec 10, 2015 4:59 AM UTC
    Posted on December 10, 2015 at 05:59

    Thanks Erwan for nice clarifications. I will refer the reference manual for using the Censorship feature. Just couple of more queries.

    1. Currently I am using PLS UDE for flash programming and this feature is available with it. How about another tool which I may use during production? Whether all the tools supporting SPC560D series provide this Censorship feature to use?

    2. Whether this censorship feature works for both code as well as data flash? Whether seperate passwords can be used for code and data memories?

    Thanks in advance.

    Mike

    Erwan YVIN
    ST Technical Moderator
    Dec 10, 2015 8:51 AM UTC
    Posted on December 10, 2015 at 09:51

    Hello Mike ,

    1)  For the tool you can use ''GangProgrammer.exe'' in PLS Directory.

    you can flash 8 Boards in parallel.

    I am checking with experts what is the best way to flash a software on SPC560D

    it is not a mass market question ;)

    to enable the censorship feature, you should do by software.

    2) Yes , it is worked in the same way for DFLASH. the DFLASH will be censured too.

         it is the same password defined in NVPWD1,NVPWD2.

    CFLASH & DFLASH will be censured.

                           Best Regards

                                             Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Jan 21, 2016 11:21 AM UTC
    Posted on January 21, 2016 at 12:21

    Hello Erwan,

    For one of the posts, you mentioned about setting following registers. Can you please explain the underlined statement in detail? If both CW and SC registers should match for values, how the statement 1) can be true?

    The best mode for your case is to use the censored mode.

    Private Flash Memory Password and censored

    1) Set NVSCC0(CW) , NVSCC1(CW) different to 0x55AA. 

        Set NVSCC0(SC) , NVSCC1(SC) equals 0x55AA.

      

        

    IMPORTANT : NVSCC0(CW,SC) must be equal to NVSCC1(CW,SC) otherwise your chip will be completely locked.

     

    Thanks in advance.

    Mike