Skip to main content
ssk
Associate III
Aug 20, 2015 4:04 PM UTC
Question

SPC560 - eMIOS

Posted on August 20, 2015 at 18:04

Hello,

I am using eMIOS module for SPC560D40L3 MCU for generating PWM. I am using default configuration for the SPCStudio project with no change to FMPLL0 and Clocks settings. My target uses 8MHz external XTAL. With this, I am trying to generate a PWM for frequency ranging from 15Hz to 600Hz. I observed that the PWM channel is not giving exact frequency PWM on the output. The difference is small at lower values but goes on increasing as the frequency rises (@ 125Hz at 600Hz). Why is this behavior for eMIOS module? Is any additional configuration required?

Thanks in advance.

Mike.
    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    Aug 24, 2015 9:29 AM UTC
    Posted on August 24, 2015 at 11:29

    Hello mike ,

    I am checking the issue with the EMIOS experts.

          Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Aug 25, 2015 2:03 PM UTC
    Posted on August 25, 2015 at 16:03

    Hello Erwan,

    Any updates on this? Your earliest help will be highly appreciated.

    Thanks.

    Mike.

    Erwan YVIN
    ST Technical Moderator
    Aug 25, 2015 3:58 PM UTC
    Posted on August 25, 2015 at 17:58

    Dear Mike ,

    i have sent an email concerning this issue.

                Best Regards

                             Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.