Skip to main content
Matthew Richardson
Associate III
Jun 11, 2018 8:15 AM UTC
Question

SPC56 5V Tolerant Logic Levels

Posted on June 11, 2018 at 10:15

I feel like I am not finding an explicit answer to this question in the errata.  I notice that the SPC56 has a 5V tolerant ADC, but I am wondering if I can use 5VDC logic for the GPIO pins?  I have some legacy 5V shift registers and I am wondering if the GPIO inputs are 5V safe...

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Jun 11, 2018 9:47 AM UTC
    Posted on June 11, 2018 at 11:47

    Hello Matthew ,

    you can find some useful information in the datasheet for SPC56EL70

    http://www.st.com/content/ccc/resource/technical/document/datasheet/7a/58/72/a0/1c/45/4a/1b/DM00070691.pdf/files/DM00070691.pdf/jcr:content/translations/en.DM00070691.pdf

     

      Best regards

                      Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Matthew Richardson
    Associate III
    Jun 11, 2018 8:22 PM UTC
    Posted on June 11, 2018 at 20:22

    I don't feel like that data sheet is explicit.  I understand that the ADC pins are 5 Volt tolerant when the ADC Reference is 5V, but I guess this is mostly for ADC register conversion reasons, not hardware?.  ADC pads are multiplexed with GPIO.  This leads me to believe that maybe the hardware is tolerant, at least prior to mux.  Based on how vague the datasheet is, it wouldn't be wise for me to assume that any of the GPIO is 5 Volt tolerant, even if the pin is tolerant when configured for ADC.  I'm not using any ADC, and I understand that there is a difference between accepted logic levels, verse actual hardware tolerance.  Is there a more definitive answer, are GPIO input pins 5 Volt TTL tolerant?

    VDD_HV_ADR    max is 6.4V

    VDD_HV_IO        max is 4.5V <- this serves as an input reference and output current source (i think).

    GPIO [Input]        max is ?