Skip to main content
Larsa
Associate II
Sep 21, 2021 10:43 AM UTC
Solved

SPC5 update can not apply GTM patches

We have just ran the update for SPC5 and on regenerating the application we get this message. What can we do to solve that?

/Larsa

0693W00000DnwBMQAZ.jpg

    This topic has been closed for replies.
    ECAST.1
    ECAST.1Best answer
    Visitor II
    Sep 22, 2021 8:46 AM UTC

    Hello,

    the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).

    Every time that the User re-generate the code, the customization are applied to the source files.

    This message is reported when the patches are no more necessary (patch code is already present in the source file) or when totally not aligned with the source file.

    If, it is in the second case, please apply the patch manually, ignoring the SPC5Studio message.

    BR,

    Emanuele

    2 replies

    ECAST.1
    ECAST.1Best answer
    Visitor II
    Sep 22, 2021 8:46 AM UTC

    Hello,

    the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).

    Every time that the User re-generate the code, the customization are applied to the source files.

    This message is reported when the patches are no more necessary (patch code is already present in the source file) or when totally not aligned with the source file.

    If, it is in the second case, please apply the patch manually, ignoring the SPC5Studio message.

    BR,

    Emanuele

    Larsa
    LarsaAuthor
    Associate II
    Sep 22, 2021 9:19 AM UTC

    That makes sense, thanks Emanuele!