Skip to main content
PChia.2237
Senior
Jun 20, 2022 4:30 PM UTC
Solved

SPC5-UDESTK not connect to SPC560B-DIS

Hi,

I have SPC5-UDESTK plug in to SPC560B-DIS board and i have activated VCP but still not connect.

If I use onBoard debbuger works, but i need to work with external SPT5-UDESTK to program my custom board, and indeed not work.

Any idea?

Thank you in advantage

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 21, 2022 8:47 AM UTC

    Hello patrick ,

    if debug is working , PLS FTDI Driver is well installed.

    Please Check your device manager if you can see the COM PORT when VCP is activated (cf screenshot)

    then check with Test Application provided by SPC5Studio

    LIN0TX and LIN0RX should be installed.

    0693W00000NsM90QAF.png0693W00000NsM8vQAF.png 

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 21, 2022 8:47 AM UTC

    Hello patrick ,

    if debug is working , PLS FTDI Driver is well installed.

    Please Check your device manager if you can see the COM PORT when VCP is activated (cf screenshot)

    then check with Test Application provided by SPC5Studio

    LIN0TX and LIN0RX should be installed.

    0693W00000NsM90QAF.png0693W00000NsM8vQAF.png 

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.