Skip to main content
Andrew Tierney
Associate
Mar 2, 2017 2:33 PM UTC
Question

SPC5-UDESTK adapter voltage source

Posted on March 02, 2017 at 15:33

I have an SPC5-UDESTK JTAG adapter here, which I am using with UDE.

Does the adapter source it's own voltage, or do I need to feed voltage from the target back to it? If so, which pin is used?

Thanks

    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    Mar 3, 2017 10:11 AM UTC
    Posted on March 03, 2017 at 11:11

    Hello Andrew ,

    Normally  , When plugged on the Board 

    SPC5-UDESTK and USB Cable.

    it should be ok.

    the booard is supplying the voltage for SPC5-UDESTK

             Best regards

                               Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Andrew Tierney
    Associate
    Mar 3, 2017 1:57 PM UTC
    Posted on March 03, 2017 at 14:57

    So it seems that I need to provide voltage from the board back to the adapter on one of the pins. I seem to have found this pin as it makes one of the LEDs on the adapter light up.

    Is there not any documentation about the pins and LEDs on the SPC5-UDESTK?

    Is there anyway to chose internal voltage? 

    Erwan YVIN
    ST Technical Moderator
    Mar 9, 2017 11:06 AM UTC
    Posted on March 09, 2017 at 11:06

    Hello Andrew ,

    Which board do you use ?

    For a discovery Board, You do not need to use 

    SPC5-UDESTK , the 

    Discovery Board contains the hw debugger by FTDI (Usb), you have just to plug the mini usb cable.

                Best Regards

                                   Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.