Skip to main content
KShar.5
Associate
Oct 3, 2022 5:44 PM UTC
Question

SPC5-UDESDK JTAG debugger stopped working after PC was rebooted.

I am setting up a development environment with SPC5-Studio, Discovery Plus Kit for SPC56 L line (with SPC56EL70L5 MCU) and SPC5-UDESDK JTAG debugger.

Initially I was able to set up the SPC5-Studio and upload an example application (LED blinker), but after rebooting my PC the UDE STK tool stopped connecting. No matter what settings I use - the result is the same, the debugger can not connect to the board. I tried reinstalling, UDE and SPC5-Studio to no avail.

To debug the problem I have connected a logic probe to the SPC5-UDESTK pins (TCK, TDI, TDO) and I see absolutely no activity on those pins when I attempt to connect with the UDE STK software.

It seems that the SPC5-UDESTK device stopped functioning correctly. The Windows OS detects the SPC5-UDESTK device correctly.

What can I do to restore the functionality of the SPC5-UDESTK device?

    This topic has been closed for replies.

    7 replies

    Erwan YVIN
    ST Technical Moderator
    Oct 5, 2022 2:15 PM UTC

    Hello Konstantin ,

    could you check your PLS USB/JTAG by FT_Prog

    https://ftdichip.com/utilities/ ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    KShar.5
    KShar.5Author
    Associate
    Oct 6, 2022 4:23 PM UTC

    Device is detected. What I should be looking at?

    0693W00000UnWYhQAN.png 

    XML template is available here: https://pastebin.com/raw/Dtbc9RAv

    KShar.5
    KShar.5Author
    Associate
    Oct 6, 2022 4:29 PM UTC

    UDE STK still doesn't connect:

    0693W00000UnWaOQAV.png 

    Connection failure report: https://pastebin.com/raw/etf6iDiq

    KShar.5
    KShar.5Author
    Associate
    Oct 6, 2022 4:31 PM UTC

    Photo of the device, connected to the EVB:

    0693W00000UnWasQAF.jpg

    Erwan YVIN
    ST Technical Moderator
    Oct 10, 2022 9:54 AM UTC

    Maybe a reset escalation

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    KShar.5
    KShar.5Author
    Associate
    Oct 10, 2022 10:04 AM UTC

    Reset escalation is hardly an answer as power cycling doesn't solve it.

    See also my initial comment, especially this part:

    ---

    To debug the problem I have connected a logic probe to the SPC5-UDESTK pins (TCK, TDI, TDO) and I see absolutely no activity on those pins when I attempt to connect with the UDE STK software.

    ---

    There is no activity on the JTAG pins when I press the "connect" in the UDE STK debugger software.

    KShar.5
    KShar.5Author
    Associate
    Oct 10, 2022 6:08 PM UTC

    Dear ST!

    Please kindly consider actually looking into the issue, rather than guessing what it could be. Please also consider reopening the support case #00165293 which you have closed without providing a resolution.

    If you need more information to troubleshoot this I would be happy to provide it.