Skip to main content
Associate II
Sep 20, 2024 7:56 AM UTC
Solved

SPC5 Studio with a different compiler

Hello, 

 

I currently have SPC560P chip which I am able to program using SPC5 Studio and Debug using SPC5-UDESTK. The compiler that I have currently selected is "FreeGCC with VLE Support" by going to the Application Configuration -> SPC560Pxx Platform Component RLA -> Build Settings.

I see the other options in the dropdown of Compiler Variant such as Hightech and GreenHills. 

The issue that I am currently facing is that I am modifying only a part of the existing code and I need to use another compiler when merging with the old code. So I was wondering if I can change the compiler to "mwcceppc" from "FreeGCC with VLE Support"  in SPC5 Studio ? If Yes, how ? 

I have added the path to "mwcceppc" in the SPC5 Studio -> Windows -> Preferences -> C/C++ -> Build -> Environment. And also the same in Project Properties. But I believe the settings in Configuration.xml will override these settings ?

Let me know if this is a possibility or not.

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Sep 24, 2024 7:42 AM UTC

Hello ,

yes , it is possible to use CDT in Makefile mode (not Makefile generated) in order to add to your own compiler.

Maybe , you need to create your C project (CDT) and import the configuration in your CDT Project.

                  Best Regards

                                 Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Sep 24, 2024 7:42 AM UTC

Hello ,

yes , it is possible to use CDT in Makefile mode (not Makefile generated) in order to add to your own compiler.

Maybe , you need to create your C project (CDT) and import the configuration in your CDT Project.

                  Best Regards

                                 Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
asnAuthor
Associate II
Sep 24, 2024 8:05 AM UTC

Correct me if I am wrong, In the case suggested by you, I will import my existing project and use my own Makefile and this will be a standalone project in SPC5 Studio. I will not be able to use PinMap Editor or Configuration.xml file correct as it is not a SPC5 C/C++ Application ?