Skip to main content
alessandro2
Associate III
Sep 27, 2016 8:54 AM UTC
Question

SPC5 studio - placing variables at fixed RAM addresses

Posted on September 27, 2016 at 10:54

Hello everyone.

I�m working on a Bolero microcontroller (SPC560D40L3) using SPC5Studio and Hightec Compiler.

I have a question related to variables to be located in RAM.

I have a set of global variables, which I need to place in RAM, at fixed addresses.

How can I do that?

Is it sufficient to declare variable as pointers and initialize them with known values?

Are there ant attributes that can be used to force variables to be located at given addresses?

Do I need to make changes to the linker script?

Thank you.

#address #variables #ram
This topic has been closed for replies.

6 replies

Erwan YVIN
ST Technical Moderator
Sep 27, 2016 1:38 PM UTC
Posted on September 27, 2016 at 15:38

Hello Alem ,

yes , it is possible

1) Change the linker file as the attachement (application.ld.backupram)

After each generation , the linker file will be overwritten

MEMORY
{
flash : org = 0x00000000, len = 256k
dataflash : org = 0x00800000, len = 64k
ram : org = 0x40000000, len = 10k
backupram : org = 0x40002800, len = 2k
}

__backupram_size__ = LENGTH(backupram);
__backupram_start__ = ORIGIN(backupram);
__backupram_end__ = ORIGIN(backupram) + LENGTH(backupram);

.standbyram : ALIGN(16) SUBALIGN(16)
{
__standbyram_start__ = .;
*(.standbyram)
*(.standbyram.*)
__standbyram_end__ = .;
} > backupram

2) After used the code section in your source code in front Variable declaration.

__attribute__ ((section (
''.standbyram''
)))

Best regards

Erwan

________________

Attachments :

application.ld.backupram : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qbAi&d=%2Fa%2F0X0000000bpF%2FS8OuetwlOGDqS6i2g8GFqB6OzpbHfrinu_YVPNlTszw&asPdf=false
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
alessandro2
Associate III
Sep 27, 2016 2:20 PM UTC
Posted on September 27, 2016 at 16:20

Hello Erwan,

many thanks for your reply. As far as I understand, looking at the modified linker script, you' ve created a ram section starting at address0x40002800, which length is 2k. First question: let's consider the following code fragment:

1.
__attribute__ ((section (''.standbyram'')))
2.
uint8_t variable_a;
3.
uint16_t variable_b;

''variable_a'' would be placed at0x40002800, right? And ''variable_b'' at0x40002802, because of the 16 bits alignment od ''stanbyram'' section, right? Second question: how do I terminate the section? Suppose I want to declare a variable after ''variable_b'', which is not placed in the ''stanbyram'' section. Third question: why is the section length 2k? Aren't we missing 4k of RAM, this way? In the standard application.ld , the RAM section has 16k length (in this case, only 12k). Thank you for your assistance.
alessandro2
Associate III
Sep 28, 2016 6:55 AM UTC
Posted on September 28, 2016 at 08:55

OK, I've done some experimenting with the linker script.

I can manage to place variables within memory sections. What I don't understand is why the microcontroller crashes whnever I try to access one the fixed address variables. If I declare a variable like:

uint8_t __attribute__ ((section (''.standbyram''))) PARAMETER1_TEST ;

and I try to access it, the microcontroller crashes. If I just remove the __attribute__ and the variable is declared as a normal variable, everything is OK. Any idea? Thank you.
Erwan YVIN
ST Technical Moderator
Sep 28, 2016 7:58 AM UTC
Posted on September 28, 2016 at 09:58

Hello Alem ,

yes it is well 16K of SRAM .. you can adjust application.ld to match with your SRAM

it was a old application based on STANDBY WAKEUP Interrupt.

i have no problem in my side

__attribute__ ((section (
''.standbyram''
))) uint8_t toto;

/*
* Application entry point.
*/
int
main(
void
) {
uint8_t message[]= 
''Hello World!\r\n''
;
/* Initialization of all the imported components in the order specified in
the application wizard. The function is generated automatically.*/
componentsInit();
/* Enable Interrupts */
irqIsrEnable();
/*
* Activates the serial driver 1 using the driver default configuration.
*/
sd_lld_start(&SD1, NULL);

toto = 2;

MEMORY
{
flash : org = 0x00000000, len = 256k
dataflash : org = 0x00800000, len = 64k
ram : org = 0x40000000, len = 10k
backupram : org = 0x40002800, len = 6k
}

the variable is well at

(Cf screenshot)

Best regards

Erwan

________________

Attachments :

2016-09-28_094530.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qUK4&d=%2Fa%2F0X0000000bni%2FUOV71dF6k3.E5XK8nC1OcFDK1kgLwHGQOuJRL6FfNOY&asPdf=false
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
alessandro2
Associate III
Sep 28, 2016 8:49 AM UTC
Posted on September 28, 2016 at 10:49

Hello Erwan, 

thanks for your reply.

Ok, I unnderstand I can adjust the ''backupram'' size.

Regarding the microcontroller crash, do nothing different than you  and I still got the problem.

Could it be related to compiler settings? (please, see my settings below).

Thank you.

0690X00000602dnQAA.jpg

Erwan YVIN
ST Technical Moderator
Oct 14, 2016 9:10 AM UTC
Posted on October 14, 2016 at 11:10

Hello Alem ,

Maybe the generation will replace automatically your application.ld

we will deliver a a way to create your own user.ld on SPC5Studio 5.1.0

or your application is too big.

          Best regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.