Skip to main content
cihaong
Visitor II
Oct 26, 2013 6:29 PM UTC
Question

SPC5 Studio and Freescale MPC5634

Posted on October 26, 2013 at 20:29

I would like to know if  SPC5 Studio and ChibiOS can be used as tool chain for Freescale MPC5634 which has similar Core to ST SPC563M:  E200z3 ?  

#spc5studio
    This topic has been closed for replies.

    2 replies

    Nickname16641_O
    Visitor II
    Oct 28, 2013 8:24 AM UTC
    Posted on October 28, 2013 at 09:24

    Hi,

    Technically, the two devices are exactly the same so the generated code can be used. I would verify the SPC5Studio license agreement however, not sure if there is something there preventing it.

    Giovanni

    Luca RODESCHINI
    ST Employee
    Oct 28, 2013 10:14 PM UTC
    Posted on October 28, 2013 at 23:14

    Hi,

    as per licence agreement accepted during the download, SPC5 studio can be used only in combination with STMicroelectronics microcontrollers.

    Is there a specific reason to keep using Freescale part numbers?

    From ST you can get equivalent products and using ST microcontrollers you gain the rights to use SPC5studio suite for free.

    if you have any specific need to facilitate the switch please let un know. Every customer is welcome @ST.

    best regards

    Luca