Skip to main content
acarn
Visitor II
Oct 10, 2019 5:16 PM UTC
Solved

SPC5-MCTK-LIB_RTM_1_1_0_web, lack of #include "pal_lld.h"?

Hello,

there's problem when trying to build the project (Regardless which of the Web Motor Control Demos I choose).0690X00000ApTKCQA3.png

The steps I made are:

1.) Import samples from application

2.) Choose one of the motor control applications

3.) Generate the SPC5 Application

4.) Build the SPC5 Application

The last step generates following error message:

./components/spc56xx_web_motor_control_component/lib/System_Drive_Params/src/Spc5xxx_MC_it.c:48:21: fatal error: pal_lld.h: No such file or directory

 #include "pal_lld.h"

Which is a bit strange, since I didn't make any changes to the configuration.

Can you please help?

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 28, 2020 4:29 PM UTC

    Hello ,

    1) MCTKLIB 1.1.0 is not compliant with SpcS5studio 5.8.1-Diadem

     There is Change Request to update the library .

    2) MCTKLIB 1.1.0 is compliant with SPC5Studio 5.8.1 (Old Version)

    http://mirrors.spc5studio.com/5.8.1/

    you can use it without updated RLA components.

    3) http://mctkcust.spc5studio.com is compliant with the last version but you need some credentials.

    to be asked in credentials@spc5studio.com

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    Oct 17, 2019 1:43 PM UTC

    Hello ,

    i think that the web site is not updated .

    i have forwarded your request to the good person.

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Czhu.844
    Visitor II
    Nov 6, 2019 6:25 AM UTC

    How about the problem? I also meet it ,help!

    Erwan YVIN
    ST Technical Moderator
    Nov 14, 2019 9:51 AM UTC

    hello ,

    after the next release of SPC5Studio , we will post a new release located in web update site

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    a-daniel
    Visitor II
    Jan 22, 2020 10:04 AM UTC

    Hello,

    Was anything done about this ?

    I have the same issue with SPC5-MCTK-LIB 1.1.0 and SPC5Studio 5.8.1 .

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 28, 2020 4:29 PM UTC

    Hello ,

    1) MCTKLIB 1.1.0 is not compliant with SpcS5studio 5.8.1-Diadem

     There is Change Request to update the library .

    2) MCTKLIB 1.1.0 is compliant with SPC5Studio 5.8.1 (Old Version)

    http://mirrors.spc5studio.com/5.8.1/

    you can use it without updated RLA components.

    3) http://mctkcust.spc5studio.com is compliant with the last version but you need some credentials.

    to be asked in credentials@spc5studio.com

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.