Skip to main content
Erwan YVIN
ST Technical Moderator
Dec 21, 2017 10:04 AM UTC
Question

spc5.drive.cloudforge.com

Posted on December 21, 2017 at 11:04

SPC5Studio 5.7.1 is available

Dear All ,

SPC5Studio 5.7.1 is available

*** Highlights ***

Here are the changes coming with SPC5Studio v5.7.1

For Selected Customers:

================

- Network bugs fixing

Use these following update sites :

http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5

http://spc5.drive.cloudforge.com/projects/spc5tools/updates

(New update Site for free GCC feature and PLS Feature)

http://hightec.spc5studio.com/

(Hightec compiler)

                  Merry Christmas

                                 Erwan

#spc58 #spc5studio #spc56 #spc57
    This topic has been closed for replies.

    11 replies

    Guglielmo Spina
    Associate
    Jan 18, 2018 11:23 AM UTC
    Posted on January 18, 2018 at 12:23

    PinMap editor for SPC570S50 is available?

    Erwan YVIN
    ST Technical Moderator
    Jan 18, 2018 3:11 PM UTC
    Posted on January 18, 2018 at 15:11

    Yes , it is ;)

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Guglielmo Spina
    Associate
    Feb 1, 2018 2:54 PM UTC
    Posted on February 01, 2018 at 15:54

    it not working fine, because when I click on PinMap editor Link error message appears:

    'Device specific model 'SPC570S50E1' not supported!'

    Erwan YVIN
    ST Technical Moderator
    Feb 2, 2018 10:25 AM UTC
    Posted on February 02, 2018 at 10:25

    Yes , it is supported

    have you installed the last version of the pinmap  ?

    Cf SPC5Studio marketplace

               Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Yalin Gurcan
    Associate III
    Jun 5, 2018 4:05 PM UTC
    Posted on June 05, 2018 at 16:05

    I have the latest version of pinmap installed from the marketplace but I still have the same problem. I'm using the SPC570S-DISP eval board.

    Patriks
    Senior
    Feb 11, 2018 12:20 PM UTC
    Posted on February 11, 2018 at 13:20

    Does SPC5 Studio support new SPC58x microcontrollers? If not is it planned to implemented support for theses controllers soon? I´ve installed the new SPC5 Studio release and would like to experience with SPC582B-DIS board.

    Erwan YVIN
    ST Technical Moderator
    Feb 12, 2018 8:42 AM UTC
    Posted on February 12, 2018 at 09:42

    Hello ,

    Please refer to the installation procedure after downloading SPC5Studio

    for SPC58x family ,it is for selected customers 

    could you send an email to

    mailto:credentials@spc5studio.com

     ?

    if the marketing guys are ok , we will send you a login/pass for spc58x support

      Best regards

           

                  Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.