Skip to main content
SV.9
Associate
Feb 12, 2024 7:29 AM UTC
Solved

SPC5 Controller is Heating and not connecting with debugger.

Hi,

We are using an SPC5 microcontroller for a motor controller application. All of a sudden, we weren't able to connect with our motor controller board, which runs on the SPC5 controller, and we also found that it was getting heated up to 36 °C.

and while checking, we found something short in the "VDD_HV_IO0" pin, and we have checked by removing all the decoupling capacitors too. Now, should I consider that the controller went off, or are there any other ways to fix or debug this issue?

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 12, 2024 1:50 PM UTC

Hi,

It seems that some current coming back from the motor might have fried the MCU...

Best Regards,

AutoDevKit Team

2 replies

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 12, 2024 1:50 PM UTC

Hi,

It seems that some current coming back from the motor might have fried the MCU...

Best Regards,

AutoDevKit Team

SV.9
SV.9Author
Associate
Feb 13, 2024 5:07 AM UTC

That is what I had anticipated. Apart from changing the MCU, are there any other options?