Skip to main content
MDupo.1
Visitor II
Dec 8, 2020 9:07 AM UTC
Solved

SPC5 code call from flash to RAM

Hi,

I've got the latest SPC5Studio 6 with all updates (gcc4.9.4) and testing on the SPC560D40L1 chip with the discovery board. So core is e200z0h VLE.

I want to manipulate the flash in my app so I need to call some code from the RAM. I added the necessary sections in the application.ld, and the necessary attribute for my method :

__attribute__ ((section (".codeinram"))) void method_in_ram()

I'm calling this method from flash code

void flash_method() {

method_in_ram()

}

All this compile correctly (no warning, no error), but this crashes during debug with invalid opcode...

I decompiled the hex, found that the flash_method content is not VLE code but PPC code !! e200z0h does not support PPC but only PPC VLE. Why is gcc creating PPC opcodes to call a method in RAM ? I tried to add longcall attribute but it does not help ...

Any help appreciated!

Thanks

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Feb 4, 2021 8:57 AM UTC

    Hello ,

    There are some examples in SPC5Studio.

    you have to create user.ld at the root of the project. (cf user.log in attachment)

    __attribute__ ((section (".codeinram"))) void gotoStandbyMode(void) {
     
    	WKUP.WISR.R = 0x00000008;		//Clear interrupt flag
     
    	if ((ME.GS.B.S_CURRENTMODE < SPC5_RUNMODE_RUN3)
    	 || (ME.GS.B.S_CURRENTMODE > SPC5_RUNMODE_RUN0)) {
    	 if (OSAL_FAILED == halSPCSetRunMode(SPC5_RUNMODE_STANDBY)) {
    	 SPC5_CLOCK_FAILURE_HOOK();
    	 }
    	 }
    }
     
    __attribute__ ((section (".codeinram"))) void gotoRunMode(void)
    {
    	 if (OSAL_FAILED == halSPCSetRunMode(SPC5_RUNMODE_DRUN)) {
    	 SPC5_CLOCK_FAILURE_HOOK();
    	 }
    }

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Giuseppe DI-GIORE
    ST Employee
    Jan 11, 2021 8:46 PM UTC

    Hello,

    did you manage to copy the code from flash to RAM before executing it ?

    could you share the application.ld ?

    Regards,

    Giuseppe

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Feb 4, 2021 8:57 AM UTC

    Hello ,

    There are some examples in SPC5Studio.

    you have to create user.ld at the root of the project. (cf user.log in attachment)

    __attribute__ ((section (".codeinram"))) void gotoStandbyMode(void) {
     
    	WKUP.WISR.R = 0x00000008;		//Clear interrupt flag
     
    	if ((ME.GS.B.S_CURRENTMODE < SPC5_RUNMODE_RUN3)
    	 || (ME.GS.B.S_CURRENTMODE > SPC5_RUNMODE_RUN0)) {
    	 if (OSAL_FAILED == halSPCSetRunMode(SPC5_RUNMODE_STANDBY)) {
    	 SPC5_CLOCK_FAILURE_HOOK();
    	 }
    	 }
    }
     
    __attribute__ ((section (".codeinram"))) void gotoRunMode(void)
    {
    	 if (OSAL_FAILED == halSPCSetRunMode(SPC5_RUNMODE_DRUN)) {
    	 SPC5_CLOCK_FAILURE_HOOK();
    	 }
    }

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.