Skip to main content
guo qiang
Senior
Aug 10, 2017 2:32 AM UTC
Solved

SP5 Studio 5.5 Problem (CAN Issue)

Posted on August 10, 2017 at 04:32

1.The CANConfig structure adds a number of field information,it have a ''fifo_rx_callback'' function point.

. Why is there a dialog box in SP5Studio that does not configure fifo_rx_callback?Causes the '' fifo_rx_callback'' function point to NULL

0690X00000607lhQAA.png

2. Building failed when disenable CAN filter.

0690X00000607kVQAQ.png0690X00000607n9QAA.png

this is a bug

Yvin.Erwan.001

‌

erwan.leray@st.com

‌

simon.scullion

‌

null
    This topic has been closed for replies.
    procolo
    procoloBest answer
    Visitor II
    Aug 10, 2017 7:46 AM UTC
    Posted on August 10, 2017 at 09:46

    Hi,

    Regarding point 1)

    Currently the FIFO is supported only on Pictus and it's going to be introduced in other platforms. You are using bolero B platform so you cannot see FIFO configurator yet but the driver already support it. In the next version FIFO configurator will be available also for your platform.

    Reagrding point 2)

    As already said, an ER is opened and issue will be solved in next release . Meanwhile, please change can_lld.c file with the attached one.

    Best Regards,

    Procolo

    ________________

    Attachments :

    can_lld.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyWR&d=%2Fa%2F0X0000000b90%2F2JWzlKWEpnxPqdzZyUBe8UFXq4G885aYzSeKIB0n8Gw&asPdf=false

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Aug 10, 2017 7:31 AM UTC
    Posted on August 10, 2017 at 09:31

    Hello Guo ,

    i am submitting an ER (Error Report) for this issue

           Best regards

                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    procolo
    procoloBest answer
    Visitor II
    Aug 10, 2017 7:46 AM UTC
    Posted on August 10, 2017 at 09:46

    Hi,

    Regarding point 1)

    Currently the FIFO is supported only on Pictus and it's going to be introduced in other platforms. You are using bolero B platform so you cannot see FIFO configurator yet but the driver already support it. In the next version FIFO configurator will be available also for your platform.

    Reagrding point 2)

    As already said, an ER is opened and issue will be solved in next release . Meanwhile, please change can_lld.c file with the attached one.

    Best Regards,

    Procolo

    ________________

    Attachments :

    can_lld.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyWR&d=%2Fa%2F0X0000000b90%2F2JWzlKWEpnxPqdzZyUBe8UFXq4G885aYzSeKIB0n8Gw&asPdf=false