Skip to main content
Patriks
Senior
Nov 25, 2014 12:18 PM UTC
Solved

[solved] Interrupt priorities

Posted on November 25, 2014 at 13:18

Hello,

Yesterday, I investigated a problem with my software project for an SPC560B. There are several calculations running on the controller and it additionally communicates over UART with a PC. When I tried to increase the UART baud rate, I got the effect that the controllers ''miss'' some bytes sent by the PC.

I found out, that reason for that effekt has something to do with the UART RX interrupt and an interrupt created by the periodical timer PIT. After the PIT causes an interrupt, the UART RX can not trigger an interrupt. I always thought that a higher priority interrupt can break the program even when another lower prior interrupt is currently running?

Best regards,

Patrik
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Apr 23, 2015 4:28 PM UTC
    Posted on April 23, 2015 at 18:28

    Hello Patrik ,

    The problem has been reproduced .

    in forcing in ivor.s, it is working.

    /* Allows preemption while executing the software handler.*/
    wrteei 1
    /* Executes the software handler.*/
    bctrl
    /* Prevents preemption again.*/
    wrteei 0

    Could you try this piece of code ''ivor.s'' ?

    The compilation switch was not taken in account.

    i am checking the platform configuration in SPC5studio

    Best Regards

    Erwan

    ________________

    Attachments :

    photo.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0VV&d=%2Fa%2F0X0000000bZm%2FItO27sKjPGzL3Ya3K0cSNAw_8by8ZlvVr186uAmJKRE&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    16 replies

    Erwan YVIN
    ST Technical Moderator
    Nov 27, 2014 8:30 AM UTC
    Posted on November 27, 2014 at 09:30

    Hello Patrik ,

    We are investigating the issue

                Best Regards

                          Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Patriks
    PatriksAuthor
    Senior
    Dec 12, 2014 6:31 AM UTC
    Posted on December 12, 2014 at 07:31

    Dear Erwan,

    Can you already give me a hint how I can avoid the described behaviour? I thought about locking other interrupts during the UART receive process. Is there a way to lock parts of the source code (e.g. an interrupt handler) that it can not be interrupted from another interrupt source?

    Best regards,

    Patrik

    Erwan YVIN
    ST Technical Moderator
    Jan 21, 2015 4:53 PM UTC
    Posted on January 21, 2015 at 17:53

    Hello Patrik ,

    Sorry for the late answer.

    osalSysLockFromISR is used to enter to a critical zone.

    OSAL_USE_IRQ_PREEMPTION is not defined (cf osal.h)

    you can try to define OSAL_USE_IRQ_PREEMPTION in your project (Platform component)

    but we have not tested this case.

    Which speed do you try to validate ?

       best regards

                    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Patriks
    PatriksAuthor
    Senior
    Jan 23, 2015 11:50 AM UTC
    Posted on January 23, 2015 at 12:50

    Hello Erwan,

    I have added a picture which shows the loss of UART data (hope it worked). The PIT interrupt raises every 100ms and can´t be interrupted from the UART RX interrupt. UART baud rate was configured as 460800.

    Best regards,

    Patrik

    ________________

    Attachments :

    pic.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyLa&d=%2Fa%2F0X0000000bZq%2FEx56LI44R7FHrFI4CPZ_DHJPwcDyMZa4VSdrVMigVak&asPdf=false
    Erwan YVIN
    ST Technical Moderator
    Jan 30, 2015 10:01 AM UTC
    Posted on January 30, 2015 at 11:01

    Hello Patrik ,

    in the default OSAL Configuration,

    PIT_0 happenned every 1 ms. (set to 1000) in OSAL

    did you try ''Preemptable ISRs'' ?

      Best Regards

                 Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Patriks
    PatriksAuthor
    Senior
    Feb 2, 2015 6:52 AM UTC
    Posted on February 02, 2015 at 07:52

    Hello Erwan,

    do you mean to set

    OSAL_ENABLE_IRQ_PREEMPTION

    in osal.h to TRUE? I never tried to change any of theses default settings.

    /*===========================================================================*/ 
    /* Module pre-compile time settings. */ 
    /*===========================================================================*/ 
    /** 
    * @brief Enables the interrupts during the ISRs execution. 
    */ 
    #if !defined(OSAL_ENABLE_IRQ_PREEMPTION) || defined(__DOXYGEN__) 
    #define OSAL_ENABLE_IRQ_PREEMPTION FALSE 
    #endif 

    For what is PIT_0 used in default configuration? Best regards, Patrik
    Erwan YVIN
    ST Technical Moderator
    Feb 2, 2015 4:58 PM UTC
    Posted on February 02, 2015 at 17:58

    Hello Patrick ,

    OSAL_ENABLE_IRQ_PREEMPTION

    is configurable on OSAL Component. (Configuration level) FALSE by default

    #if OSAL_ENABLE_IRQ_PREEMPTION
    /* Allows preemption while executing the software handler.*/
    wrteei 1
    #endif
    /* Executes the software handler.*/
    bctrl
    #if OSAL_ENABLE_IRQ_PREEMPTION
    /* Prevents preemption again.*/
    wrteei 0
    #endif

    PIT_0 is used for 1ms tick (os-less) If you think that the Tick is too heavy, you can try to enable this feature. Best Regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Nickname16641_O
    Visitor II
    Feb 3, 2015 1:53 PM UTC
    Posted on February 03, 2015 at 14:53

    Hi Patrik,

    At which baud rate you start to experience the issue?

    Giovanni

    Patriks
    PatriksAuthor
    Senior
    Feb 3, 2015 2:59 PM UTC
    Posted on February 03, 2015 at 15:59

    Hello Giovanni,

    I tried three baud rates. It worked with 57,6kb/s, but not with 460,8kb/s and 128kb/s.

    Best regards,

    Patrik
    Patriks
    PatriksAuthor
    Senior
    Apr 22, 2015 2:19 PM UTC
    Posted on April 22, 2015 at 16:19

    Hello!

    Once again, I have problems with interrupt priorities (the issue I started with this topic has never been solved).For my current project, Ihave a very high priority ISR which must preempt all other ISRs. I tried different priorities and settings within the source code, butI wasn´t able to get this behavior.

    Therefore, I set up a small demo project for SPC56xL Discovery Board (based on SPC56EL OS-Less Demo Application from SPC5 Studio)

    Within this application, I integrated two PIT timer interrupts (channel1 and channel2). One interrupt handler gets a high priority (8) and the other one a low priority (2). I expected, that the high priority preempts the lower priority. But the higher priority interrupt is only executed when the lower priority isn´t running.

    For better understanding, I attached a picture. In this picture, signal D6 represents the lower prior interrupt, D4 the higher prior interrupt. The two pins are set at the beginning of the corresponding ISR and cleared at the end of ISR.

    To be sure that it isn´t a problem with my interrupt handlers, I also created the ISRs using the SPC5 Application Configuration with activated ''Preemptable ISRs'' option. Nevertheless, I got the same result as with my ''own'' interrupt handlers.

    These are the interrupt handlers in osal_cfg.c:

    /*===========================================================================*/ 
    /* Module ISRs. */ 
    /*===========================================================================*/ 
    /* 
    * ISR_1 ISR function (vector 61). 
    */ 
    OSAL_IRQ_HANDLER(vector61) { 
    OSAL_IRQ_PROLOGUE(); 
    /* ISR code here.*/ 
    Task_10us(); 
    /* Resets the PIT channel 0 IRQ flag.*/ 
    PIT.CHANNEL[2].TFLG.R = 1; 
    OSAL_IRQ_EPILOGUE(); 
    } 
    /* 
    * ISR_2 ISR function (vector 60). 
    */ 
    OSAL_IRQ_HANDLER(vector60) { 
    OSAL_IRQ_PROLOGUE(); 
    /* ISR code here.*/ 
    Task_100us(); 
    /* Resets the PIT channel 0 IRQ flag.*/ 
    PIT.CHANNEL[1].TFLG.R = 1; 
    OSAL_IRQ_EPILOGUE(); 
    } 
    /*===========================================================================*/ 
    /* Module exported functions. */ 
    /*===========================================================================*/ 
    /** 
    * @brief Generated initialization code. 
    * 
    * @special 
    */ 
    void osal_cfg_init(void) { 
    INTC_PSR(OSAL_VECTOR_ISR_1)=INTC_PSR_ENABLE(INTC_PSR_CORE0, 8); 
    INTC_PSR(OSAL_VECTOR_ISR_2)=INTC_PSR_ENABLE(INTC_PSR_CORE0, 2); 
    } 
    /** @} */

    Additionally, OSAL_ENABLE_IRQ_PREEMPTION in osal_cfg.h is set TRUE

    #if !defined(OSAL_ENABLE_IRQ_PREEMPTION) 
    #define OSAL_ENABLE_IRQ_PREEMPTION TRUE 
    #endif

    What is the reason for the described behavior? And how I have to configure my system toactivate preemption of lower priorities by higher priority ISRs?

    Best regards,

    Patrik

    ________________

    Attachments :

    scope_72.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Vk&d=%2Fa%2F0X0000000bZo%2FrJoqsMF2nqhS.6_N.508vRWfiqkn9aZhUOcTRN0gUM4&asPdf=false