Skip to main content
gl2
Associate III
Jun 29, 2015 11:09 AM UTC
Solved

[Solved] How can I use the Arduino microseconds delay of SPC-560P?

Posted on June 29, 2015 at 13:09

I have this sensor HY-SRF05 with 5 pins. In Arduino using the function delayMicroseconds () to manage the operation of the sensor so:

Arduino code:

/*

Tested with HY-SRF05, HC-SR04

Assuming a room temp of 20 degrees centigrade

The circuit:

* VVC connection of the sensor attached to +5V

* GND connection of the sensor attached to ground

* TRIG connection of the sensor attached to digital pin 12

* ECHO connection of the sensor attached to digital pin 13

*/


const
int
TRIG_PIN = 12;

const
int
ECHO_PIN = 13;


void
setup() {

// initialize serial communication:

Serial.begin(9600);


pinMode(TRIG_PIN,OUTPUT);

pinMode(ECHO_PIN,INPUT);

}


void
loop()

{

long
duration, distanceCm, distanceIn;


// Give a short LOW pulse beforehand to ensure a clean HIGH pulse:

digitalWrite(TRIG_PIN, LOW);

delayMicroseconds(2);

digitalWrite(TRIG_PIN, HIGH);

delayMicroseconds(10);

digitalWrite(TRIG_PIN, LOW);

duration = pulseIn(ECHO_PIN,HIGH);


// convert the time into a distance

distanceCm = duration / 1 / 2 ;

distanceIn = duration / 74 / 2;


if
(distanceCm <= 0){

Serial.println(
''Out of range''
);

}

else
{

Serial.print(distanceIn);

Serial.print(
''in, ''
);

Serial.print(distanceCm);

Serial.print(
''cm''
);

Serial.println();

}

delay(1000);

}

Of SPC560P how can I do? The board does not handle microseconds. Best regards Gianluca.
    This topic has been closed for replies.
    gl2
    gl2Best answer
    Associate III
    Jul 1, 2015 10:05 AM UTC
    Posted on July 01, 2015 at 12:05

    Ok, the function osalThreadSleepMicroseconds it works.

    Thanks. 

    Best regards

    Gianluca

    7 replies

    Erwan YVIN
    ST Technical Moderator
    Jun 29, 2015 11:57 AM UTC
    Posted on June 29, 2015 at 13:57

    Hello Gianluca ,

    you have to use :

    osalThreadSleepMilliseconds(100);

    Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    gl2
    gl2Author
    Associate III
    Jun 29, 2015 1:10 PM UTC
    Posted on June 29, 2015 at 15:10

    But 100 milliseconds are 10,000 microseconds. I'd need 2 and 10 microseconds.

    Best regards

    Gianluca

    Erwan YVIN
    ST Technical Moderator
    Jun 29, 2015 2:31 PM UTC
    Posted on June 29, 2015 at 16:31

    Sorry ,

    it is a bad copy-paste You can use the osal macro

    #define osalThreadSleepMicroseconds(usec) osalThreadSleep(OSAL_US2ST(usec))

    Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    gl2
    gl2Author
    Associate III
    Jun 29, 2015 7:00 PM UTC
    Posted on June 29, 2015 at 21:00

    Yes I know. Sorry for bad formatting in the last message, I do not know how it happened. Thanks.

    Best Regards

    Gianluca

    Erwan YVIN
    ST Technical Moderator
    Jun 30, 2015 8:10 AM UTC
    Posted on June 30, 2015 at 10:10

    No Problem ;)

    Every people (Customers & Moderators) are struggling everyday on this forum based on Sharepoint solution ;)

    Best regards

     

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    gl2
    gl2AuthorBest answer
    Associate III
    Jul 1, 2015 10:05 AM UTC
    Posted on July 01, 2015 at 12:05

    Ok, the function osalThreadSleepMicroseconds it works.

    Thanks. 

    Best regards

    Gianluca

    Erwan YVIN
    ST Technical Moderator
    Jul 2, 2015 7:51 AM UTC
    Posted on July 02, 2015 at 09:51

    Hello Gianluca ,

    Good news ;)

       Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.