Skip to main content
270284440
Associate II
Jul 1, 2015 1:48 AM UTC
Solved

[solved]DSPI Rx FIFO question

Posted on July 01, 2015 at 03:48

I am programming on pictus dspi module, I have queries describe below:

/********************************************/

    DSPI(module).PUSHR.R = nCONT|DSPIx_CTAR0|nCS+ucDIN;

    while(DSPI(module).SR.B.RFDF == 0); 

    //Point A  

    DSPI(module).SR.B.RFDF = 1;   

    //Point B

/********************************************/

question are:

1) Read POPR should be inserted at Point A or Point B

2) From reference manual , I understand that RFDF is a flag indicating Rx FIFO is not empty, if I dont add any read DSPI_POPR code here, Will Rx FIFO be flushed to no entry level?

Thanks!

#dspi-pictus
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 2, 2015 2:03 PM UTC
    Posted on July 02, 2015 at 16:03 Hello Chu , 1) i recommend you to use RX FIFO Counter The RXCTR is decremented every time the DSPI_POPR is read POPR should be inserted at Point A RFDF shows that the interrupt is served Example from SPC5Studio (spi_lld.c)

    void
    spi_serve_dspi_rfdf(SPIDriver *spip) {
    osalSysLockFromISR();
    /* Emptying the RX FIFO.*/
    while
    ((spip->rx_cnt > 0) && (spip->dspi->SR.B.RXCTR > 0)) {
    uint32_t frame = spip->dspi->POPR.R;
    if
    (spip->rx_ptr != NULL) {
    if
    (spip->dspi->CTAR[0].B.FMSZ < 8)
    *spip->rx_ptr8++ = (uint8_t)frame;
    else
    *spip->rx_ptr16++ = (uint16_t)frame;
    }
    spip->rx_cnt--;
    }
    /* Interrupt served.*/
    spip->dspi->SR.B.RFDF = 1;

    ''In the interrupt service routine, RFDF must be cleared only after the DSPIx_POPR register is read.'' 2) RFDF is setwhile the RX FIFO is not empty. if you set 1 it will be reset. Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 2, 2015 2:03 PM UTC
    Posted on July 02, 2015 at 16:03 Hello Chu , 1) i recommend you to use RX FIFO Counter The RXCTR is decremented every time the DSPI_POPR is read POPR should be inserted at Point A RFDF shows that the interrupt is served Example from SPC5Studio (spi_lld.c)

    void
    spi_serve_dspi_rfdf(SPIDriver *spip) {
    osalSysLockFromISR();
    /* Emptying the RX FIFO.*/
    while
    ((spip->rx_cnt > 0) && (spip->dspi->SR.B.RXCTR > 0)) {
    uint32_t frame = spip->dspi->POPR.R;
    if
    (spip->rx_ptr != NULL) {
    if
    (spip->dspi->CTAR[0].B.FMSZ < 8)
    *spip->rx_ptr8++ = (uint8_t)frame;
    else
    *spip->rx_ptr16++ = (uint16_t)frame;
    }
    spip->rx_cnt--;
    }
    /* Interrupt served.*/
    spip->dspi->SR.B.RFDF = 1;

    ''In the interrupt service routine, RFDF must be cleared only after the DSPIx_POPR register is read.'' 2) RFDF is setwhile the RX FIFO is not empty. if you set 1 it will be reset. Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    270284440
    270284440Author
    Associate II
    Jul 3, 2015 1:53 AM UTC
    Posted on July 03, 2015 at 03:53

    Hi, erwan.

    I debug by UDE yesterday,

    It is true that I cannot write 1 to clear RFDF flag if I dont read POPR data first.

    It is better to check '' RX FIFO Counter'' as you suggest.

    Thank you so much!