Skip to main content
ivancolla9
Associate III
Jan 19, 2016 4:06 PM UTC
Question

Self-Test Control Unit RAM test type

Posted on January 19, 2016 at 17:06

Good morning,

I have a techincal question regarding the Self Test Control Unit of  SPC56EL60 microcontrollers.

It seems from the documentation that the unit performs various types of self-tests for the micro, including ram memory test (MBIST). I cannot find what type of memory test the unit perform: abraham, galpalt or others? I am misunderstanding the unit capabilities?

Thanks.

#test #stcu #ram
This topic has been closed for replies.

3 replies

Erwan YVIN
ST Technical Moderator
Jan 20, 2016 8:42 AM UTC
Posted on January 20, 2016 at 09:42

Hello Ivan ,

I am checking with SOC Functional Validation team.

   Best regards

              Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Erwan YVIN
ST Technical Moderator
Jan 21, 2016 4:03 PM UTC
Posted on January 21, 2016 at 17:03

Hello Ivan ,

Here is the feedback from Verif Team.

1)      MARCH LR14  (Four backgrounds)

2)      Address decoder delay test

3)      Mask Bit test 

4)      csn test

Best regards

                     Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ivancolla9
Associate III
Jan 22, 2016 9:04 AM UTC
Posted on January 22, 2016 at 10:04

Well, this is all the information I needed.

Thank you very much for the help,

Ivan