Skip to main content
TBles.1
Associate
Aug 17, 2022 9:45 AM UTC
Solved

RX_Callback at SPC560P - Disp

I want to know when or how exactly the RX callback function is triggered on the SPC560P - Disp Discovery board.

I have created the function at the low level driver at the serial configuration and see it also in serial_lld_cfg. I have defined it afterwards.

I want to work in asynchronous mode to avoid blocking. I can also receive single bytes with the function sd_lld_read().

But the callback function is never called or executed. what is the reason?

Actually I would like to receive more than just one byte which is why I want to use the callback function as an interrupt.

Can anyone help me here?

Thanks

Timo

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Aug 30, 2022 1:42 PM UTC

    Hello ,

    for this,

    i recommend to use a RTOS (real Time os) (Example : Chibios or FreeRTOS)

    1 thread for RX/TX Serial

    1 thread for other stuff.

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    3 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Aug 30, 2022 1:42 PM UTC

    Hello ,

    for this,

    i recommend to use a RTOS (real Time os) (Example : Chibios or FreeRTOS)

    1 thread for RX/TX Serial

    1 thread for other stuff.

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    POlss.3
    Visitor II
    Oct 4, 2022 7:42 AM UTC

    Hi 

    I´m also trying to achieve the same goal, using the "SPC58ECxx_RLA FreeRTOS SERIAL Test Application for Discovery". Serial from MCU to PC is ok via USB to RS232 Converter.

    I fail to see how the interrupt of received serial message should be configured (Used in "Main.c")

    I would very much appreciate your help!

    I´m new to the SPC5 environment but I´m eager to learn! 

    Thanks in advance!

    Best Regards

    Peter

    TBles.1
    TBles.1Author
    Associate
    Oct 17, 2022 12:17 PM UTC

    Sorry I dont exactly know, I get my Program running without FreeRTOS