Skip to main content
stefanodimascio9
Associate III
Feb 15, 2016 12:06 PM UTC
Question

Register allocation

Posted on February 15, 2016 at 13:06

Hello, 

I'm using SPC5 studio with the high-tec tool chain for SPC56EL70L5. I'd need to set the linker in such a way that one out of 32 general purpose register won't be never used by the compiler because I need it for some assembly code lines. Could you tell me what kind of directives do I have to use?

Thank you in advance for the help
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Feb 22, 2016 2:25 PM UTC
    Posted on February 22, 2016 at 15:25

    Hello Stefano ,

    i do not know if Hightec can handle that.

    the simplest way is to Save/Restore  registers that you use ..

      Best regards

              Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.