Skip to main content
Visitor II
Mar 19, 2024 10:17 AM UTC
Question

Recommendation of PART no of MCU with datasheet which will meet automotive standard

I need one part no of MCU which will meet automotive standard and have MCU 32-bit ARM Cortex M0+ RISC 512KB Flash 2.5V/3.3V 32-Pin, 512 KB flash Memory, 64 MHz clock rate and operating temperature is -40 to 125 °C.

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Mar 19, 2024 10:39 AM UTC

    Welcome @Nabanita_23, to the community!

    No device with your specification and Automotive certification is currently available.

    Does it answer your question?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.