Skip to main content
rpoon
Associate II
May 29, 2019 9:09 AM UTC
Solved

Reason of delay 200 ms after sd_lld_write function.

Hello

Is there any specific reason behind putting this delay, if yes than what it is?

I want to manage time in my application so i tried to reduce the delay but in that case I am not able to transmit data properly.

below is the given function

 sd_lld_write(&SD1,CMD2,(uint16_t)(sizeof(CMD2)/sizeof(CMD2[0])));

osalThreadDelayMilliseconds(200);

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 28, 2019 12:34 PM UTC

    Hello rewatee ,

    it is better to use the Runtime IO component in SPC5Studio

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 28, 2019 12:34 PM UTC

    Hello rewatee ,

    it is better to use the Runtime IO component in SPC5Studio

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    rpoon
    rpoonAuthor
    Associate II
    Jul 16, 2019 12:19 PM UTC

    Hello Erwan

    I am facing same problem with the Runtime IO component as well. I have set the configuration parameter in Runtime io environment.

    I am using "function ioWrite(int fd, const void *buf, size_t count)" for data transmission.

    can you please provide some sample code?

    Regards

    Rewatee