Skip to main content
This topic has been closed for replies.

2 replies

Erwan YVIN
ST Technical Moderator
Aug 28, 2023 3:33 PM UTC

Hello ,

According the the AN 

This device is family compatible with the L9678,
L9680 and L9679P devices: it has been designed as extension chip of the others, but if configured in the right
way it can be used standalone.

what do you mean about Self-Triggered ?

               Best regards

                           Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Visitor II
Sep 11, 2023 9:34 PM UTC

I have a similar if not the same question. I have been tasked with doing a design in a few weeks that needs to fire Pyro Fuses when current sensors assert their overcurrent fault flag. I've been told that this needs to be on the order of 50uS so a SPI message would be too slow. From what I can tell the L9679P and L9679e can be told through SPI to deploy and will wait for during the timeout period for a trigger signal.

It looks to me that this could be done using the FENL pin. Could the DCSx pins also cause the L9679P to trigger once a deploy command is sent?

Is there a better way to get this quick of trigger on an overcurrent?

Rob