Skip to main content
JHsu.14
Associate
Aug 13, 2026 1:47 AM UTC
Solved

Programming guide for SR5E1E570C30F01X

Hi,

 

Good day.

This is the third party programming manufacturer.

We are searching out the programming guide of SR5E1E570C30F01X because our customer requires this series for programming, and they will use our programming handler for production.

 

Now, We need these matirals for progarmming development.

  1. Keil C PACK file and sample code (I didn’t see it in Keil website)
  2. The programming guide for SR5E1E570C30F01X includes commands and flow and related information about programming.

Please let me know if need to sign NDA.

Thank you.

Jack

 

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Sep 24, 2026 12:19 PM UTC

or SR5E1E570C30F01X, I recommend using StellarStudio, the official ST development environment for Stellar SRx microcontrollers:

StellarStudio — official ST page 

Suggested workflow:

  1. Install StellarStudio from the official ST page.

  2. Select the exact target device, SR5E1E570C30F01X, if it is available in the installed device-support package.

  3. Create or open the project through StellarStudio.

  4. Build the application and use the programming/deployment flow provided by StellarStudio for the selected target.

  5. Before production programming, confirm the required programming interface, board connections, device configuration, and programmer flow in the device-specific documentation or with your ST FAE.

Keil has not been tested for this device and flow, so please do not assume that a Keil device pack, debugger configuration, or programming procedure is supported.

   Best regards

                       Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Sep 24, 2026 12:19 PM UTC

or SR5E1E570C30F01X, I recommend using StellarStudio, the official ST development environment for Stellar SRx microcontrollers:

StellarStudio — official ST page 

Suggested workflow:

  1. Install StellarStudio from the official ST page.

  2. Select the exact target device, SR5E1E570C30F01X, if it is available in the installed device-support package.

  3. Create or open the project through StellarStudio.

  4. Build the application and use the programming/deployment flow provided by StellarStudio for the selected target.

  5. Before production programming, confirm the required programming interface, board connections, device configuration, and programmer flow in the device-specific documentation or with your ST FAE.

Keil has not been tested for this device and flow, so please do not assume that a Keil device pack, debugger configuration, or programming procedure is supported.

   Best regards

                       Erwan

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.